Part Number: PCM1753 Dear Sirs,
I have a question.
The description of Zero Detect condition on page 16 of the data sheet is as follows.
If the data for a given channel remains at a 0 level for 1024 sample periods (or LRCK clock periods), a zero-detect…
Part Number: PCM1803A Other Parts Discussed in Thread: PCM1753 Dear Sirs,
My customer asked us about Terminal Capacitance of BCK pin for PCM1803A and PCM1753.
Please let me know it.
Best Regards,
Y.Hasebe
Part Number: PCM1753 Other Parts Discussed in Thread: PCM5121 , PCM5100A , PCM1774 Dear Technical Suppot Team,
I have an issue of pop noise on PCM1753 when power-on and power-off(on⇒off⇒on⇒off⇒on・・・).
This is old device. Could you tell…
Other Parts Discussed in Thread: PCM1753 as default after power up, the pcm1753 has left justified audio interface mode.
In the register description 24 or 16 bits is mentioned ( one should asume 16bit frame as well).
However in the format figure, bck 48x…
Other Parts Discussed in Thread: PCM1753 Hi Team,
The customer is using PCM1753. In his design, he tests the SNR value and it is only 72dB. He does a test. He removes the LEFT_LPF and RIGHT_LPF circuit ,and connects two 10uF capacitance to 7 pin and 8 pin…
Part Number: PCM1753 Hi,
I am wanting to use this DAC with a 3.3V micro controller and my concern is that its a 5V device. There is no mention from what I can see that there are pull up resistors, or that there are not. I am nervous the 5V ends up on…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1753-Q1 , PCM1754 , PCM1753 , Hi Expert,
We are getting a problem with this hardware control IC and getting too much distortion over audio because of format mismatch, we have pulled down the FMT…
Part Number: DS90UB949-Q1 Other Parts Discussed in Thread: PCM1753 Hello TI team, I have been working with DS90UB949-Q1 and an audio DAC PCM1753. The application is such that, the user's laptop is connected to the serializer using an HDMI connection and…
Other Parts Discussed in Thread: PCM1753 , PCM1754 Hi all Would you mind if we ask PCM1753 and PCM1754? How much is Group Delay? We could not find it on the datasheet. Kind regards, Hirotaka Matsumoto