Hi Kato-san,
We currently do not have any EOL planned for the PCM1742. Though, that is an older product that was replaced by the lower-cost, marginally higher performance PCM1753/4 family. The PCM175x family is a very high volume device, and will be…
Kuramochi-san,
The PCM1755 has the same zero detection functionality as the PCM1753. The only difference is that zero flag outputs are open-drain on the PCM1755.
Thanks,
Paul
Hi Kuramochi-san,
The PCM1754 will enforce a 64x oversample regardless of the SCLK/LRCK ratio. Only the PCM1753 will automatically change the ratio. This means that the THD+N will be the same with either 128×fS or 256×fS. Only the sample rate will change…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1753 Dear Sirs,
My customer asked us about pin capacitance specification for PCM1753 and PAM1754.
1.Does the PCM1753 / 54 have SPECification of the output load capacitance of the VCOM pin…
Part Number: PCM5100A-Q1 Other Parts Discussed in Thread: PCM5100A , PCM5122 , PCM1753 Hi
Just want to confirm that what are the sample frequencies of PCM5100A? Does it support 22Khz or must be 44Khz or some frequency value else? Customer used 22Khz…
Hi George,
Will the PCM need to drive the speaker directly, or will they have an amplifier? If they require a device that can drive the speaker as well then you will need to look at some of the TAS devices.
The DAC features two channels, left and…
Hi Paul ,
Thanks for your explanation.
it seems I should change PCM1754 to PCM1753 to minimize this noise by Soft Mute or add LPF on the PCM1754 output.
Do you have any suggestions about LPF for PCM1754 ?
Thanks.
Franco
Other Parts Discussed in Thread: PCM5100A , PCM1753 , PCM5242 Hi Team, I couldn't find Audio Interface Timing in PCM5100A datasheet. Is there audio interface timing requirement like the following PCM1753? (PCM1753 datasheet page 6) Best Regards, Yaita…
Other Parts Discussed in Thread: DS90UB928Q , PCM1753 Dear Technical Support Team,
I have questions about DS90UB928Q.
1.)
Could you tell me the maximum spec of tSES and tONS?
"Figure 10. Output State (Setup and Hold) Times" shows tSES and tONS…