Part Number: PCM1864EVM Hi Expert,
I found the same problem as the below link, I checked the TAS1020 firmware version is 3.04 and sampling rate is 48KHz.
If the version is wrong, can you send the right firmware to me? Thanks!
e2e.ti.com/.../2267012
…
Part Number: PCM1864EVM Other Parts Discussed in Thread: PCM1864 , TIDA-01454 Hi all,
I had one PCM1864 CMB (TIDA-01454) Rev A on hand.
But I could only get the Rev B schematic from below link. However, I found some changes as above red circle when referred…
Other Parts Discussed in Thread: PCM1864EVM , PCM1864 TI,
I have a setup where the PCM1864evm has 4 channel microphone in. When I set up the EVM with the included USB-I2X cable to connect to the computer, I see one device.
The PCM1864 is sending data…
Other Parts Discussed in Thread: PCM1864EVM Hi everyone,
We bought one PCM1864EVM, and wants to use it as an external sound card to record 4-ch Microphone inputs on a Windows PC.
After installing Purepath console, we can find two PCM1864EVM under the…
Hello,
Our customer is using I2S format inside TDM.
Since I could not reach your mail box, so I have sent design information to Brian Donoghue.
Also, PCM1864EVM SW DL is not approved yet.
Regards,
Mochizuki
Part Number: PCM1864 Other Parts Discussed in Thread: , PCM9211 Hi team,
I've received the following questions regarding PCM1864EVM. Can you please answer the questions?
Configuration : 1KHz (1WATT) SINE WAVE input -> PCM1864EVM -> SPDIF output…
Hi,
which version we use is processor_sdk_rtos_k2g_4_01_00_06; the demo we use is realtime_demo_bios ;The PCM1864 PCB board we use is designed by ourselves ;we use ti PCM1864EVM circuits as reference ;when we test , there are a lot of problems …
Other Parts Discussed in Thread: PCM1865EVM , PCM1861EVM , PCM1864EVM , PCM1862EVM , PCM1863EVM Hi all, Would you mind if we ask PCM1863EVMGUI? In order to get PCM1863EVMGUI, I tried to request PCM1863EVMGUI on the website. However, the following shows; Also, we…