Other Parts Discussed in Thread: PCM2705C , PCM2704C , DIR9001 , PCM2704 We are planning to use one of the parts listed above (PCM2704C / PCM2705C) in a desktop speaker with a USB input. Please confirm if these parts will allow an end user to control the…
The device descriptor can be modified through the SPI port (PCM2705C/7C); this descriptor programming function is only available when PSEL and HOST are high as you did. More functional details can be found in section 9.5.1 USB Interface
Please check the…
Part Number: TPS65981 Other Parts Discussed in Thread: PCM2705C TPS65981_RCLAMP0582_CONNECTIONS.pdf
Hello,
We have a board design that uses both a TPS65981 and PCM2705C to provide 5V, 3A charging and USB audio from an Ipad. All prototype/breadboard testing…
Part Number: PCM2704C Other Parts Discussed in Thread: PCM2705C Hi team, My customer wants to use PCM2704C. Does it work by default setting without external ROM? Some models want to eliminate ROM to reduce costs. And, if it can use without ROM, how to terminal…
The PCM270xC does not require a specific driver. Please clarify: You are using the PCM2704C or the PCM2705C? Only the 2704C supports the external ROM.
Can you verify the voltage on your test points (JP9 and JP12)? On my EVM both lines are 3.3V, so I believe…
Part Number: LM49370
Dear TI-er
My customer want bidirectional I2S to PCM converter.
I saw the post with link below.
AN-1591 LM49370 PCM/I2S Bridge
He will design bidirectional usb to PCM converter.
TUSB4041i <-> PCM2705C <-> LM49370(or TLV320AIC3212…
Hi, Brian,
The PCM2900C is a simple USB-Audio codec that is able to send USB audio through stereo analog outputs. If only analog audio output is required, maybe a USB DAC could be selected, like the PCM2705C. Either the '2900 or '2705 will be recognized…
R. B.
I'm very sorry for the confusion.
Actually volume HID status can be controlled through SPI on PCM2705C and PCM2707C. But it is unable to control the digital interface volume.
I think the digital interface volume can be controlled from software…