Part Number: PCM2904 Hi team,
The customer's requirement is as below:
headphone-->USB AUDIO CODEC--->usb speaker
He wants to get the audio signal from the headphone interface of PC, then he needs to output the audio signal through USB.
Can PCM2904…
Part Number: PCM2904 Other Parts Discussed in Thread: PCM2906C Our contract manufacturer is in possession of a large quantity of PCM2904's that they would like to use up. I have a board that was originally designed for the 2904, but Windows is unable…
Part Number: PCM2904 Hi,
Should the active low pass filter be added to the signal output path if using VOUTL and VOUTR as the headphone output ? In addition, is a click sound heard if using PCM2904 without the active low pass filter ?
Best regards, Ka…
Part Number: PCM2904 Other Parts Discussed in Thread: PCM2906B , Hi Team,
As stated in SLAZ036A, the inter-channel phase difference can only be solved by application software. While in SLEL056, it seems that PCM2906B has fixed this issue.
However, the PCM2906B…
Here are some of them.
You can search under this site: Audio USB converters product selection | TI.com
PCM2906C data sheet, product information and support | TI.com
PCM2900C data sheet, product information and support | TI.com
PCM2902C data sheet, product…
Part Number: PCM2904 Other Parts Discussed in Thread: PCM2906C , HID2 Hi Team,
How do I enable the HID function of the PCM2904?
I guess I need to enable the HID end-point since the control end-point is the default setting.
But I don't see the way to…
Part Number: PCM2904 Hi,
Could you please help to review the schematic and board layout for PCM2904 ? Please contact me as I could share them via a private message on e2e.
Best regards, Kato
Part Number: PCM2904 Tool/software: Linux Hi. I've issue with PCM2904, I've created pcb with 2 microphones lines, pcb connected to linux machine with ubuntu 16.04, kernel 4.8.0-51, system properly detect device, but alsamixer can't set mic levels, with…
Part Number: PCM2904 Tool/software: Linux Hi support-san! I ask you how to access PCM2904 in Ubuntu Qt Which protocol should I use for to access PCM2904? If possible, please show me sample code or any information.
note) I have already access the PCM2904…
Part Number: PCM2904 Dear fellow developers,
I am currently designing a system which includes the PCM2904. In order to optimize the power managemant subcircuit (and to stay USB compliant) I would need the enumeration status of the device. I am particulary…