Would suggest to download and install 5400 chip support library from the link: http://www.ti.com/tool/sprc132
and refer the example sprc132\C54xxCSL\examples\c5400\dsk5416\csl\mcbsp\mcbsp1
1. You may create a copy of an example project and then make…
Other Parts Discussed in Thread: PCM3002 Hey all, I am trying to interface a PCM3002 to an F28335 via McBSP. My sample rates are being supplied by the ePWM of the F28335 and they are: LRCIN = 41.85 kHz, Bitclock = 1.33 MHz, and the sysclock = 10.75 Mhz…
naveen francis said:
My question is, can the data from pcm3002 get to the processor via mcbsp?
Yes. The connection between the PCM3002 and the C5416 would be with the McBSP interface.
naveen francis said:
If so, does the data come serially…
Hi,
You can refer to the attached excel for a high level summary of these parts.
AIC3254 driver should work with the PCM3070.
8838.AIC-PCM products.xlsx
Regards.
Tommy,
You are right, its a Spectrum Digital board. A friend of mine has written this code. I could paste whats written in the .h files here if that would give you a clearer idea.
#define
CHIP_5416…
Hi Nicolae,
See attached list for the differences.
3122.AIC-PCM products.pdf
The 2 devices have different voltages, hopefully the list will help.
Regards,
Peter
Hi Yuki,
I have attached here our CODEC products for you to peruse, you can click the part number to go to the product folder.
Take a look which will suit your customer requirements, these are currently active devices.
Let me know if you have other…
Other Parts Discussed in Thread: PCM3002 Hello,
I'm working on implementation of comb filter in tms320c5416(codec pcm3002).Initially I have written C code(posted below) for ONLY ONE FIR filter.But its not working when I checked on CRO. Can any one tell…
Hi Lex,
Attached here is a high level summary of some of our codec devices, this is by no means exhaustive.
AIC-PCM products_scale.pdf
For the full list you can look under this link which is only sorted for audio codec.
https://www.ti.com/audio…
I'm not aware of other language support for the documents.
The codec used on the DSK5416 is the PCM3002. Information regarding the DSK5416 can be found at Spectrum Digital's support site for the DSK.