Part Number: PCM3168A Tool/software: Hi
I am using IMX 8QuadXMax Applications Processors (MIMX8QM6AVUFFAB).
I need to connect two pcm3168a-q1 to in how i connect it, how i connect the pins.
Thanks & Best Regards
Dov Segal
Senior Hardware Engineer …
Part Number: PCM3168A Tool/software: Hello,
I am working on designing an ADC buffer circuit for this codec, and I cannot for the life of me discern a substantive difference between the two recommended circuits in the data sheet: fig 58 and 59.
Obviously…
Part Number: PCM3168A
Tool/software:
Hi expert,
I did some tests with different configuration about struct snd_soc_dai_driver, the results are as below:
configuration one:
static struct snd_soc_dai_driver pcm3168a_dais[] = {
{
.name = "pcm3168a-dac…
Part Number: TDA4VM Other Parts Discussed in Thread: PCM3168A Tool/software: Hi ,
Hardware platform:J721EXSOMG01EVM + J721EXCP01EVM
Software: ti-processor-sdk-linux-edgeai-j721e-evm-09_02_00_05
The board uses pcm3168a codec connected through McASP10 [AXR0…
Hi,
I have confirmed with one of my colleagues that this is a known bug with the device - when the PCM3168A is in any mode with TDM, the OVF pin does not work as expected and stays low. The OVF register works as expected. We are working on updating the…
Part Number: PCM3168A Problem description: Turn on the 48V DC phantom power supply of the MIC input interface (the current sensitivity is -56dBu, and the problem still exists at other low sensitivities). When the interface is plugged and unplugged, an…
Part Number: PCM3168A Other Parts Discussed in Thread: PCM3168 We are the facing issues while integrating pcm3168a codec driver.
Target device and version details as follows:
Kernel version : - 4.19.35
CPU : - i.MX6Q
Based on https://bootlin.com/blog…