Hi Shyam,
Here are logs from both good and bad boards.
Thanks!
Fullscreen
bad_log.txt
Download
keelung@xps:~$ minicom -w -D /dev/ttyUSB0
Welcome to minicom 2.7.1
OPTIONS: I18n
Compiled on Aug 13 2017, 15:25:34.
Port /dev/ttyUSB0…
Part Number: TDA4VM Other Parts Discussed in Thread: UNIFLASH Hi,
The applications run well after I configure environment variables at uboot prompt,while the applications run incorrectly after rebooting.It's really strange because I do save the environment…
Hi,
I think I have loaded uboot from OSPI and loaded filesystem from eMMC.But I'm not sure if I have made it.Would you please help me check about it?The boot log and environment variables are posted below.
Regards!
HJ
Fullscreen
5432…
Hi Keerthy,
Thanks for your response.
By using commands, there was no issue in reboot(sd booting), but there was still an issue in nfs booting.
After 15 trials of your commends in above, the issue was gone even in nfs booting.
Could you please…
Part Number: PROCESSOR-SDK-J721E We are using Jainto 7 board for our usecase. When i2cdetect command is executed, it shows 8 channels from 0 to 7. I n the attached document, there is an i2c tree diagram. In the i2c tree, we only see only 6 buses. Please…
Part Number: TDA4VM
Hi,
After flashing eMMC according to the thread https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-jacinto7/latest/exports/docs/linux/How_to_Guides/Target/How_to_flash_emmc_device.html ,I try to load it manually from u…
Part Number: DRA829V Other Parts Discussed in Thread: DRA829 This is using the 7.0 Linux SDK for the DRA829/J7 device. The customer is attempting to load Ethernet firmware on RF5 main core (j7-main-r5f0_0-fw) on J7 EVM. Based on the serial log from Ethernet…
Hi Lucas,
Also we found same errors for display while using direct DisplayPort-PisplayPort connection. Boot log: Welcome to minicom 2.7.1 OPTIONS: I18n Compiled on Aug 13 2017, 15:25:34. Port /dev/ttyUSB0, 18:41:42 Press CTRL-A Z for help on special…
Hello Brijesh ,
So, I looked into the steps and found that my problem wasn't what I did but the first command in step-4. I opened the install_to_sd_card.sh file and found that it start to install some part of the vision apps files. Instead of launching…