Other Parts Discussed in Thread: PCM5310 We are testing a design that uses the TI PCM5310 CODEC and have run in to some issues with the analog outputs.
1. When we send the output of DAC12 to LO1L and LO1R (register 24 contains 01110111, registers 25 and…
Other Parts Discussed in Thread: PCM5310 In looking at the datasheet for the PCM5310, I see two operating temperature ranges mentioned in the datasheet:
It is listed as -25 to + 85 on page 2 of the data sheet in the table labeled Recommended Operating …
Hi Archie,
6 stereo inputs is a lot. The only part I can find that supports that is the PCM5310. This part does not have any DSP capabilities however. The TLV320AIC3262 has a miniDSP that is configured with PurePath studio, a graphic design environment…
(Register 13, headphone short-circuit protection enable/disable), bit 5 is shown to be SHCR and bit 1 is shown to be SHCL. The function of SHCR/SHCL is not listed anywhere in the documentation. What is the function?
Page 45, SRCR & SRCL - Reset Short…
Other Parts Discussed in Thread: PCM5310 Hello,
Are the VCOMAD, VCOMDA, VREFAD1 all 1/2 power supply outputs (or are they inputs)?
If they are outputs, what are their driving strength in mA?
I'm using single supply OPAMp I/O circuit, so may I connect…
Other Parts Discussed in Thread: PCM5310 , TPS65270 Hi,
I'm using PCM5310 for 4CH audio IN and OUT. I have external out of band noise filters (active 2nd order, fc=24kHz and pasive RC fc~30kHz). Power supply is clean, I have decoupling capacitor pairs…
Other Parts Discussed in Thread: PCM5310 Hi
I am designing a small audio DSP system with 4 input and 4 output channels using a PCM5310. For space and power consumption reasons, I have chosen a DSP with only one I2S interface.
As I understand so far,…
Part Number: AM5718 Other Parts Discussed in Thread: AM5728 , PCM5310
Hi TI Audio Champs
We'd like to ask you about McASP config when the system clock is connected to PCM codec without AM5718.
Based on AM5728 evm, Customer trying to implement mcasp…
Other Parts Discussed in Thread: PCM5310 Hello,
I'm working with the PCM5310 codec and I have found a problem when I try to configure an ADC in slave mode. If I configure it in master mode, then I obtain the I2S output signal in the DATA line of the…