Part Number: PGA2505 Other Parts Discussed in Thread: PGA2500 Tool/software: Hi Team,
This is Rohit Gupta from Applied Electro Magnetics Pvt. Ltd. We are currently working on a project that requires susceptibility compliance in accordance with MIL-STD…
Part Number: PGA2505 Tool/software: I assume that the PGA2505 is normally configured as a SPI device, but could you please tell me what mode of operation it will be in if SPI communication is not performed?
Does it operate with a fixed gain Amplifier…
Part Number: PGA2505 Tool/software: Dear
Can the PGA2505 support an unbalanced microphone input
(unbalanced input methods: PIN3->NC, PIN1->GND, PIN2->IN) Similar to this circuit, there are currently three phenomena: 1. Connecting this unbalanced input…
Part Number: PGA2505 Tool/software:
Why is the voltage here 0.6V? Shouldn't it be 0V? Is it because of bias voltage? But isn't the bias voltage of chip PGA2505 ± 0.08mV?
Part Number: PGA2505 Tool/software: I need to put more than of these on a design that has other SPI devices and a processor that runs at 3V3. From the datasheet and evaluation board design it looks like 3V3 level SPI signals work fine going from the processor…
Part Number: TCA39416 Other Parts Discussed in Thread: PGA2505 , SN74LVC1G125 , SN74AHC1G125 Tool/software: I need to put more than one PGA2505 into a design that has other SPI devices and a processor that runs at 3V3. From the datasheet and evaluation…
Part Number: PGA2505 Tool/software: Hello,
I'm looking at the power supply design for my board and considering whether the PGA2505 really needs a split rail or whether it can be run from a single +5 supply?
Regards,
Dan
Part Number: PGA2505
Tool/software:
Hello,
After an over-range event occurs, how long is the OVR pin held high? I am assuming that it is transient, i.e., only held high as long as the input voltage is greater than the set threshold and will have…
Part Number: PGA2505 Other Parts Discussed in Thread: OPA1637 Hello support team,
The problem here is from our customer.
They met some bottlenecks with PPGA2505 in products, and needs your comments:
PGA2505 had max +-5V(VA+, VA- 5V power supply…