Other Parts Discussed in Thread: PLL1705 Hi All,
I would like to ask a question on the sheet 11 - VIC page of EVM6437 schematics.
What is VIC used for? There are chiefly two components on the page:
1. PLL1705 - 3.3 V Dual PLL…
Other Parts Discussed in Thread: TAS5727EVM , PCM1808 , PLL1705 , TAS5727 Hello!
I'm using home-made amplifier board, similiar to TAS5727EVM. i2s data comes from PCM1808 ADC and PLL1705 (48 kHz, 256 fs MCLK) and looks normal in logic analyzer. I'm…
Other Parts Discussed in Thread: PCM1801 , PLL1705 Hello everyone, I ran into some issues while working with the PCM1801 16 bit Stereo ADC (Datasheet: http://www.ti.com/lit/ds/symlink/pcm1801.pdf ) The chip was set up as show on page 17 of the datasheet…
Other Parts Discussed in Thread: OMAP-L137 , TLV320AIC3106 , PLL1705 I am using Zoom OMAP L138 from LogicPD.
I want to set the sampling frequency of the codec which is AIC3106 to 96kHz.
How is it going to be done. I need to use AIC306 in dual…
Other Parts Discussed in Thread: PLL1705 Hi,
I would like to configure AIC3106 in my EVM OMAP L137/c6747 to have a sampling rate of 8KHz. I tried the following, but it doesnt seem to work. Any suggestions?
page 0. register 2=0xAA - means SampRateDiv…
Hello Evgeniy:
I am now looking at the clocking to the TAS5086.
What is the purpose of the PLL1705?
Have you taked a close look at your clocks going to the TAS5086 and do they conform to the criteria in the datasheet?
What sample rate are…
Other Parts Discussed in Thread: OMAP-L137 , PLL1705 Hi can someone help me? I’m using OMAP-L137 EVM board, and I am using the example code from the web. when I tried to get the value of the ADC I found that the value is greater than what it should be…
Other Parts Discussed in Thread: PLL1705 , TMS320C6747 Hi,
I am using UDP with the audio_edma_c6747.prj - the aim is to transmit audio (using ping and pong buffering) via UDP to another device (PC) that is connected to the DSP evaluation board (EVM…
Hi,
I am using UDP with the audio_edma_c6747.prj - the aim is to transmit audio (using ping and pong buffering) via UDP to another device (PC) that is connected to the DSP evaluation board (EVM OMAP L137/ c6747) via the ethernet cable.
When I configure…