Part Number: PROCESSOR-SDK-AM62A Tool/software: Hi,
I am using the MCU to generate pulses for my application. I want the MCU to continue operating even when the main processor enters sleep mode.
To achieve this, I considered using MCU-only mode .…
Hi Sajan,
Sajan Saji said: I tried optiflow app and derived a pipeline from it. Works well with 3280x2464.
Do you mean you actually have a 4K display on AM62A and you have a 4K hdmi screen connected to the EVM and this entire setup worked fine? This…
Part Number: PROCESSOR-SDK-AM62A
Tool/software:
Hello,
How to modify the output frames and implement inference that averages recognized classes across multiple frames or relates them to a time interval.
Best Regards, Sajan
Part Number: PROCESSOR-SDK-AM62A Other Parts Discussed in Thread: SK-AM62A-LP Tool/software: Hi TI Experts,
I’m currently working on enabling Falcon boot mode on the SK-AM62A-LP platform using TI Linux SDK 9.2 along with the tisdk-edgeai-image . As…
Part Number: PROCESSOR-SDK-AM62A
Tool/software:
Hello. TI experts
I have a question about Yocto-build in PSDK-LINUX-AM62A-10.00.00.08.
In the section of 1.2.3.2. Build Steps, I'm wondering if this command is correct or not. Please review this…
Part Number: PROCESSOR-SDK-AM62A Tool/software: Hi team,
We have questions about LPDDR4 ZQ training sequence by TI SoC.
ZQ calibration is one of DDR training. In general, controller need to issue a “ZQ start” command and “ZQ latch command ” command…
Part Number: PROCESSOR-SDK-AM62A Tool/software: Hi :
I am working on am62axx-evm TI 10.00.02 yocto source code, not the sdk environment. And now I want to enable the fitImage and ramdisk.
Through the code , I found that, maybe this file ./oe-core…
Hi Chau,
Chau Le said: Can you verify if MCR has been installed properly?
Yes, MCR is installed properly.
Chau Le said: Can you also try to install the latest version of the DCC Tuning Tool V3.2 and see if the issue persists?
First I tried 3.20…
Part Number: PROCESSOR-SDK-AM62A Tool/software: Hello, I generated pth file by refering following URL. * https://github.com/TexasInstruments/edgeai-tensorlab/issues/7 * Used "$ python3 tools/train.py configs/yolov8/yolov8_s_syncbn_fast_8xb16-500e_coco…
Part Number: PROCESSOR-SDK-AM62A Tool/software: Dear supporters,
I would like to use SDK 08_02_0x_0x image for my AM62A.
But in the SDK page, there are only 9.x and 8.6.
Is there any way to use SDK 08_02_0x_0x for AM62A?
Thank you in advance…