Part Number: PROCESSOR-SDK-AM62A Tool/software: Hi, I'm trying to compile yolov8 custom model. I can generate onnx and prototxt files and I'm trying to complie these models under edgeai-tidl-tools. However, I'm facing following error. 1. Envirnment. SDK…
Part Number: PROCESSOR-SDK-AM62A Hi Expert,
Linux kernel version in the last AM62A SDK release
Is the kernel version 6.1.x ?
Is there any documentation describing this?
Thanks
Daniel
Hi Xingyun,
xingyun zhao said: Does 06, 24, 04, 00 in the first 32bit in the figure correspond to the first data in H3A-AF?
It looks like.
xingyun zhao said: If so, should we read?
I believe it is in little endian.
xingyun zhao said: Whether…
Part Number: PROCESSOR-SDK-AM62A Hey there,
I'm trying to deploy a face detection tflite model on AM62A using TIDL-OSRT . The two outputs of my model are the score of face existence in the image and 6 approximate facial keypoint coordinates plus facial…
Hi Tommy,
Glad to hear you are using AM62A and it is our pleasure to help you using it. See my comments/answer below:
Tommy To said: The chip runs Aragon OS and supports Max 2 TOPS.
We do not support Aragon OS for AM62A. More about our SDK offering…
Part Number: PROCESSOR-SDK-AM62A Tool/software: We are encountering several issues with the AM62A 9.2 TIDL toolchain that require support:
1. Bin Inference :
When exporting the bin in the X86 Container, using PCxxx.out for inference results in a Segment…
Part Number: PROCESSOR-SDK-AM62A Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hello, TI experts.
I want to clarify the sysconfig version in PSDK10.0.0.5 AM62A Firmware builder.
In the .component_versions_am62a_env file, the version…