Part Number: PROCESSOR-SDK-AM62X
Tool/software:
Dear support:
Now I have encountered the operation optimization problem of the AM62x M4F kernel program, I would like to ask for advice。
(1)The test found that the program running on the M4F core…
haibin xiao said: 4,M4F core crash;
Can you please tell when the M4F crash, what error message do you see on console?
Also are you able to halt the core when issue happens?
Which example are you trying to run?
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hello TI expert,
I imported the example into CCS, but I do not know how to make it run.
Should just take it as R5 core app?
Part Number: PROCESSOR-SDK-AM62X Tool/software: I need to debug the miniPCIE. The required functions include USB, UART, and SPI. Among them, USB and UART need to utilize the 4G function, while SPI needs to use the LoRa function.How should I configure…
Part Number: PROCESSOR-SDK-AM62X Tool/software:
Hi,
While browsing PROCESSOR-SDK-AM62X Software development kit (SDK) | TI.com
The latest mcu_plus_sdk is version 11_01_00_16 while the version I can download from ti.com/secureresources/AM62X-RESTRICTED…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hello Team,
MCAL Package: MCAL_SitaraMPU_09.01.00
As per SWS_Mcu_00134, The MCU module shall provide at least the values MCU_POWER_ON_RESET and MCU_RESET_UNDEFINED for the enumeration Mcu_ResetType.…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hello, I am trying to test read/write GPIO Port Expanders via i2c on the EVK AM62X-LP but I am not sure if the command is right, considering the address 0x22 0x23.
Could you please explain, for instance…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hi,
I am using the TIMEOUT register to get time-delimited messages on ECU. as per TRM 1 unit of the register value is 1 baud cycle. but when I calculate as per each bit time I observing erroneous timeout…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Brenda Diaz
Hi,
Thanks for reaching out. Could you please share the following information:
SOM schematic and layout (shared through private E2E message if not publicly available)
AM62x power estimation…
Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: AM625 Tool/software: Hi - I'm investigating a problem where some of our AM625 boards are not booting. One possible cause could be a problem with the DDR. Is there a tool, or similar, I…