Part Number: AM62A7-Q1 Other Parts Discussed in Thread: INA3221 , TS3A227E , BQ25890 , SN65DSI83 , SN65DSI86 , LM90 , HD3SS3220 , BQ25980 , TFP410 , TPS65219 , TPS65132 , TAS2552 , DP83869 , ADS1015 , AM62A7
Hello expert:
Right now I used the falcon…
Part Number: AM3351 Other Parts Discussed in Thread: TPS65217
Tool/software: Linux
Hi Team,
The TRM for AM335x shows AM3351 can be operated at 300MHz and 600MHz. I am unable to configure it to 600MHz.
[ 1.808783] random: fast init done [ 1.822032…
Sikai Lu said: Do you have any logs of good board? Or do you have any preivous version of SDK that runs well?
RTOS 0801 runs well and 0801 R core log show as follows:
[MCU2_0] 450.310362 s: CIO: Init ... Done !!! [MCU2_0] 450.310434 s: ### CPU Frequency…
Part Number: AM625 Hello,
I am using AM62xx-evm and want to interface the OV5647 PI cam with it. I am using the SDK 09.02.00.
In SDK I found the k3-am62x-sk-csi2-ov5640.dtso.I have modified the file as follows:
// SPDX-License-Identifier: GPL-2…
If you follow the link in the post I made previously, it shows this:
Note: The UBL binary found in the prebuilts section of the SDK is
will run the processor at 456MHz. If your part will not run at that
speed please use the UBL binary that ships…
Willis said:
Sorry, I should have clarified- the BLEv1.1 SDK includes an updated version of KeyFobDemo. The application functionality is generally the same but updated to work with the v1.1 stack.
Thanks for clarifying. I was mislead by…
Other Parts Discussed in Thread: SYSBIOS I am using the TI Integra processor and I am developing my DSP code using the Code Composer Studio v5.1 application. I generate my DSP application and get the resulting ELF formatted .out file from Code Composer…
1) I assume FPGA board is powered separately, right?
What is the POR sequence you are using?
Yes. We are powering on the FPGA after all the voltages on AM3894 processor
module are stable. Since 0.9V is the last voltage in processor module…
Other Parts Discussed in Thread: TPS65910 The Linux kernel of Android SDK has the internal processor rtc as source. I have tps65910 rtc driver working too as rtc1. Can a linux expert help me with the following issue? How can I call inside rtc-omap the…
Hi James,
The Robust RVC should work properly on those different stages.
It is started as soon as bootloader loads the vision SDK firmware.
Once Robust RVC is started, it will never stop. So, it works for (2) and (3) conditions.
The reverse gear…