Hi Kim,
But why do you want to specify the initphase? Typically for the full frame scaling operation, it is set to 0. Are you setting it to 0 for both host emulation mode and target mode?
Regards,
Brijesh
Part Number: AM4377 The latest version of PROCESSOR-SDK-LINUX-RT-AM437X currently available is 09.03.05.02 (released on December 13, 2024). Is there a release scheduled for a newer version? If so, when is it expected to be released?
For comparison,…
Part Number: PROCESSOR-SDK-J784S4 Tool/software: Hi Team,
I'm not able to run below OpenCV applications available in Linux SDK:
opencv_annotation
opencv_waldboost_detector
Environment used:
OS: Linux TI Linux SDK version: 10_01_00_05 OpenCV…
Part Number: PROCESSOR-SDK-AM67 Tool/software: I am using the PROCESSOR-SDK-AM67 (09.02.00.04) environment, and I am outputting video via LVDS.
When I check the kernel log in this environment, the following logs are continuously output at a certain…
Part Number: PROCESSOR-SDK-J784S4 Tool/software: Hi Team,
I'm not able to run below OpenCV applications available in Linux SDK:
opencv_interactive-calibration
opencv_visualisation
Environment used:
OS: Linux TI Linux SDK version: 10_01_00_05…
Part Number: J721EXSOMXEVM
Hi Team,
I recently raised a request for sf probe failing in u-boot. E2E1655549 but am not able to access the ticket for some reason. So raising a new request. We checked the issue is resolved on the latest SDK 11.02.00…
Hello Kota,
Your assumption is correct.
Kota Takata said: Based on the code, it seems that the tool for DRA72x is also compatible with DRA71x.
Best,
Josue
Part Number: PROCESSOR-SDK-C667X Tool/software: TI-RTOS I am using rapidio over one 6678 dsp, and when I perform an atomic operation I get completion code 3. Other operation is performed ok.
I read the KeyStone Architecture Serial Rapidio Uses guid…
Hi Victor,
This thread is beginning to delve into other questions than the smp_affinity question. Please open another E2E thread about the new topics.
I will update this thread if there are any changes in the smp_affinity JIRA ticket.
Best, Jar…