Part Number: J721EXSOMXEVM Hi,
recently I have upgraded to ti-processor-sdk-linux-j7-evm-07_02_00_07 and ti-processor-sdk-rtos-j721e-evm-07_02_00_06. Once the upgrade has been done, I have flashed the SD card following the instructions and I could run…
Part Number: DRA750
Tool/software: Linux
Hi all,
I am working on getting hypervisor up on DRA75X board based on Processor-SDK, xen 4.10. Xen is up but I kernel is crashing(dom0).
I get,
of_irq_init: children remain, but no parents [ 0.000000…
Part Number: AM5728 Tool/software: TI C/C++ Compiler Hi Forum;
We are working on custom board which based on AM572x Evaluation Module. There is some hardware difference from AM572x Evaluation Module. The biggest difference we have 1 GB DDR3L RAM (2x512MiB…
I do not want to promote a particular desktop search and do not want to disparage yours, so I will leave it at that.
NDK 2.1 came with an SDK for a different processor's EVM, the C6472. I do not know when it will be released more broadly and I do not…
Part Number: AWR1443 Other Parts Discussed in Thread: UNIFLASH Hi
I am trying to capture demo by AWR1443
But it's my first time to use AWR1443 and CCS, so I failed at the first step.
In the guide mmwave_sdk_user_guide (1).pdf
Section 3. 4. 2.…
Part Number: AM5728 Other Parts Discussed in Thread: BEAGLEBOARD-X15 , , PMP Tool/software: Linux Hello,
I have some problems in setting up the tftp boot on the am572xx board.
The following shows the last part of the setup.sh sequence when restarting…
Hi Jeff,
what modules are loaded using the "lsmod" command?
Ans: $ lsmod
module size used by
It's not shown any module.
Are you using the prebuilt kernel from the SDK or did you build yourself. Ans : We are not using prebuilt kernel image…
Hi kemal,
Thank you very much for your support. I want to enable UART5 in my kernel so that I could make use of this port for RS485 communication. I am using AM4378 processor, and linux-4.1.6+gitAUTOINC+52c4aa7cdb-g52c4aa7 with sdk "ti-processor-sdk…
Hello Benoit, Manisha,
Unfortunately, all is still not well. An entry at /dev/video0 exists but I am not able run the simple yavta test.
I enabled debug and ran yavta, and v4l2-compliance. Here is the output:
root@am437x-evm:~# yavta -c10 -fYUYV…
1. I did not find a "Rules.make" anywhere. I did find a Makefile.rulse deeply buried under the source directory and looked at it with cat, as follows:
DaVinci-PSP-SDK-03.21.00.04/src/kernel/linux-03.21.00.04$ cat ./arch/um/scripts/Makefile.rules # …