Hi
I am currently using SDK 7.00 for am335x board.I am able to build kernel and flash to SD card using Software guide.
But the rootfs build is READ-ONLY . Not sure why it is Read-only.Please help if I am missing any steps.
Attaching the logs …
Part Number: AM5708 Hello all,
I'm working on a custom board which is based on AM5708 booting on a NAND.
Previously I was working with processor-sdk 06_03_00_106 which is providing linux-ti-stagging 4.19 kernel, system working fine with device…
Hi Keerthy J
Here are the log files:
Davinci2.txt, this is a log showing the situation we end up with GMAC not being able to lock and ending up blocking the entire device (I.E. no serial, no PRU’s etc etc etc)
Log (1).txt, this is running with…
Part Number: AM4378 Other Parts Discussed in Thread: AM4372 Tool/software: Linux I have a custom AM4378 board based on the AM437X-SK EVM. There is a Micron eMMC device (MTFC4GACA) connected to the mmc0 interface.
The eMMC is not detected by Linux. …
Yan Liu said: Does this mean that these two values are still not large enough?
We have seen that happen, can depend on unpowered breakaway torque of rotor magnets to stator laminations. Check the lock rotor flag is not enabled at any point for SPM or…
Part Number: WL1837MOD Tool/software: Linux Hi Sir
We used Processor SDK 2.0.1 with kernel 4.1.3 and follow below wiki to do driver porting.
processors.wiki.ti.com/.../WL18xx_Platform_Integration_Guide
We can see Waln device after executing "ifconfig…
Lisa,
I think we're getting somewhere. I have DSP/BIOS 5.x examples, but no SYS/BIOS examples:
Could you track down what component should install them? I've put my installed component list below.
Thanks, Adrian
*** System properties…
Background:
Custom board Processor: AM4379BZDNA100 Linux distro: TI PROCESSOR-SDK-LINUX-AM437X v2.00.00.00 (Linux v4.1.6) Main com port: UART1 Boot mode[4:0]: 10100b MMC0, USB_MS(USB1), USB_CL(USB0), MMC1 UniFlash : Running on Win7 PC Linux build environment…
I have narrowed the issue down to we are not properly detecting the TLV320AIC3106 chip as it is connected the same as the JAMR2.1 board.
On a kernel where I don't have this issue I see this:
usbcore: registered new interface driver snd-usb-audio…
Hi ,
My customer came across an issue about oops issue.
SDK version: ti-sdk-am37x-evm-06.00.00.00
HW: customer's board
When they test the board, it will report oops issue sometimes.
The log as follows:
kernel BUG at mm/slab.c:3057…