Other Parts Discussed in Thread: AM5728 Hi,
We are using sitara am5728 processor based custom board , we are connecting ili9341 lcd to processor using spi serial interface. We are able to see TI logo at boot time and we are able to push data from user…
Hello Pavel,
I see.. I will check the TRM you mention. Thank you for this useful information. Now I understand more about SPI to ethernet data transfer concept with TI processor. I am just a beginner in embedded linux development and doing it alone…
Below is problem report from a customer who is trying to use CCS v5.5 to connect to DRA7x on a Linux machine
---------------------------
I just installed vision SDK with the relevant updates to CCS 5.5 and trying to connect to EVE processor/s in order…
JESD204B UltraScale Hardware Demo.pdf Gregory,
TI does not but Xilinx has a reference design that might help you. Attached is a description of this firmware. You should be able to download the complete design from their website.
Regards,
Jim
Hi Geraldine,
I took a look at the Processor SDK install, and the PDK sub-product. I see that the OSAL functions are indeed defined in that example source file, as you mentioned above. I'm not sure why these functions are being defined in an example…
Part Number: AM625 Hello,
I am using AM62xx-evm and want to interface the OV5647 PI cam with it. I am using the SDK 09.02.00.
In SDK I found the k3-am62x-sk-csi2-ov5640.dtso.I have modified the file as follows:
// SPDX-License-Identifier: GPL-2…
Hello,
Can you please be more specific while asking questions. In this case, you need to provide processor name and DVSDK version. Typically you can find u-boot and ubl binaries inside the DVSDK or PSP SDK releases.
Thanks
Brijesh
Hi,
Anybody knows the solution ? Well, I have been looking at syslink which takes care of communication between A8 and M3(HDVICP2) processor to find something like CMEM_getPhys on DM365 SDK. The CMEM is still present on EZSDK but it is just for DSP…
Hi, Farrukh:
For processor SDK 5.x, the Weston version is 2.0.0 and it is built through yocto on rocko branch.
There are two major differences between the ABB build and TI build based on the weston.log.
1. Different libgbm
Please refer to the libgbm…
Other Parts Discussed in Thread: AWR1642 , AWR1843 , AWR6843 , AWR2944 , UNIFLASH , SYSCONFIG , AWR2243 , AM2732 , AWR1243
⇐ Back to Main FAQ Thread : [FAQ] PLEASE READ : mmWave Forum Guidelines and FAQ Thread
This Thread addresses FAQ in context…