Part Number: PROCESSOR-SDK-TDAX
Hi,
I want to load a baremetal binary to specific Address on userspace and execute the binary via kernel module.
I got mmap fail if I use 68.2K binary or larger size.
How can I find the suitable memory address for…
Part Number: PROCESSOR-SDK-TDAX Hi TI
There're request from Many customers regarding Yocto SDK Build.
They have downloaded the latest version, and checked most of the contents related to Git error. They're fixing it and doing it. If fixed a few…
Part Number: PROCESSOR-SDK-TDAX Other Parts Discussed in Thread: TDA4VM
VHWA has totally 6 drivers in the PDK and each driver requires many DMA channels to do transfers. In addition to one main ring, each channel requires two additional rings, one for…
Part Number: PROCESSOR-SDK-TDAX Hi Guys,
Greetings. I have an issue. I need the source-file vcop_fft_npt_16ix16o_cn.c for debugging. Unfortunately this file isn't available in www.ti.com/.../PROCESSOR-SDK-TDAX as well as installed. Could you send me…
Part Number: PROCESSOR-SDK-TDAX Hi Guys,
Greetings. We need your help. Customer is working with EVE on TDAx and missed a source code in Radar SDK 03_08_00_00. They can not debug in FFT Functionality. Normally it should be available once this is installed…
Part Number: PROCESSOR-SDK-TDAX Dear TI Team,
We are using Processor SDK Radar for developing Cascade and Satellite Radar Configuration with AWR12xx (as Radar FE) TDA2x/TDA3x device (for Data processing). While checking the Processor SDK Radar found…
Part Number: PROCESSOR-SDK-TDAX Hi Champs
There's a request that Customer wants to get achieved their goal.
They're using the TDA3x Vision SDK 3.02 version.
The usercase is the object detection in vip_single_cam_object_detection2.
The max resolution…
Part Number: PROCESSOR-SDK-TDAX Hi,
I have a python script that exports 3 kernels of the same module. I want one generated include file for the module, so I pass the module name as both include_subpath and include_filename when creating a KernelExportCode…
Part Number: PROCESSOR-SDK-TDAX Hello all,
In related to the previous thread ( https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1040112/processor-sdk-tdax-openvx-graph-performance-analysis-in-tiovx-psdk ), I have few queries…
Part Number: PROCESSOR-SDK-TDAX Hello,
I follow the steps to build the Processor _SDK-Radar,and try to display the routine 6, that is, null source (sd/network) input + radar FFT (eve1) + null (sd/network).But there is no target in the display result…