Part Number: AM3352 Other Parts Discussed in Thread: PROFIBUS Hello, do we have a reference design for Profibus MBP interface? Does MBP need a special transceiver?
Regards, Holger
Other Parts Discussed in Thread: PROFIBUS , AM3359 Tool/software: Code Composer Studio Hi All,
I need help on profibus slave application installation on TI board AM3359.
I have downloaded img and binary from TI website.
am335x-evm-linux-rt-06.03.00.106…
Part Number: ISO35T Other Parts Discussed in Thread: PROFIBUS , ISO1176T , ISO1450 , , ISO35 Hi sir,
Whether that ISO35TDW supports profibus or not. I am sure that supports rs485 but we need to make sure to know about the profibus support of that chip.
profibus…
Part Number: DAC8740H Other Parts Discussed in Thread: PROFIBUS I am now using DAC8740H to realize PROFIBUS PA application on Pressure sensor.
Now I can receive frame from PROFIBUS PA bus correctly, I can check it in my MCU as UART_OUT is connected to the…
Part Number: TMDX654IDKEVM Other Parts Discussed in Thread: PROFIBUS Hi guys,
I have the TMDX654IDKEVM board and after startup it is running in to a kernel panic error.
And I am getting also an unhandled exception EL2 when it is not a panic error.
So,…
Part Number: PROCESSOR-SDK-AM65X Other Parts Discussed in Thread: PRU-ICSS-INDUSTRIAL-SW , PROFIBUS Hi TI,
I just have a quick clarification regarding the AM65x, as I'm in the planning stages of an industrial project for which the AM65x appears to have…
Part Number: DAC8740H Hi Team,
My Customer is working with DAC8740H, and wanted to have a source code example for Profibus-PA using DAC8740H. Do we have a source code example that can be shared?
Thanks in advance.
Renan
Part Number: AM2432 Other Parts Discussed in Thread: PROFIBUS Hi TI experts,
The AM243X has two PRU subsystem and one of them has 6 RSIC core. If I want program the 6 core for custom function,such as UART.
How to design the AM243X chip physical pin map…
Part Number: AMIC110 Other Parts Discussed in Thread: PROFIBUS ,
Hi,
EVM board: iceAMIC110
SDK: PRU-ICSS-Profibus_Slave_01.00.02.01
The customer ran Profibus slave demo and console display below menu:
Profibus Application Running... I - Change inputs S -…
Part Number: AM3359 Other Parts Discussed in Thread: PROFIBUS , TMDSICE3359 ,
Tool/software: Code Composer Studio
How to set up Profibus slave AM335x ICE 1.0 EVM with master PLC S7-300 ? I have not clear how to configuration AM335x ICE 1.0 EVM (ICE) EVM . Because…