Part Number: BQ78350 Other Parts Discussed in Thread: BQ76920 , , TIDA-00792 , , BQ769200 , TIDA-01093 Dear ,
Could you please help to check the circuits of several TI chips?
Especially for BQ79620 and BD78350, I measured that there is a 0.4V difference…
Part Number: LM51231-Q1 Other Parts Discussed in Thread: LM5122 Tool/software: Hi TI Team,
I am currently working on a boost converter design using the LM51231-Q1 with the following specifications:
Input Voltage: 12V
Output Voltage: 36V…
Here i have attached the revised code and its response. No problem i will ask in general forum and see if TI employee can help me solve this issue. Its too much annoying for me to solve this issue as i am trying to troubleshoot this issue from last two…
Hello,
I'm working on a with a Texts Instruments ICEv2 evaluation board using SYS/BIOS Industrial SDK 2.1.1.2.
The application consists of a recompiled Beckhoff stack, slitly modified to used latches in the DC unit.
I initially tested the slave…
Hi experts,
The demo application is working now, but it does not detect any video in (I connected a SD video input on daughter board) , any ideas??
Thanks in advance !!!
loading kernel modules... *** Bootargs Validated for mem param *** *** Bootargs…
Hello all,
I am facing issues in mounting through nfs.
The output of printenv is as follows and i have kept the board in dhcp mode:
bootdelay=4 baudrate=115200 setboot=setenv bootargs $(bootargs) bootamd=nboot 0x80700000 0 0x500000;bootm bootfile…
Part Number: TMS320DM368 Tool/software: Linux Hi all,
I have copied Deinterlacing algorithm v2.0 from IPNC RDK to DVSDK 4.02.
Application is also using JPEG encoder and H264 Encoder in High profile.
Kernel reboots after going into VIDENC1_process…
Part Number: TMS320F28069 Other Parts Discussed in Thread: UNIFLASH , CONTROLSUITE Tool/software: Code Composer Studio Hi,
I'm using CCS 6.2 and F28069. Compiling and debugging works fine without any issue, however trying to program with UniFlash I…
Other Parts Discussed in Thread: AM5728 I'm trying to mount flash drive in linux with initramfs on Sitara AM5728 EVM board. I've create my tiny filesystem and build kerenel with initfs. But when I plug flash drive in USB port, nothing happens. I've configured…