sorry we do not make UHF RFID tags (for about 7 or 8 years now) - we do make HF RFID laundry tags (see RF-HDT-DVBB or RF-HDT-DVBE)
usually an application like this (laundry) is needing high power readers and larger antennas (either freq band)
check…
Hello Thorsten,
This is a very difficult application, and it may not be feasible with HF RFID which are the only tags we offer that fits your form factor requirements.
HF RFID is dependent on magnetic fields, so placing tags on or even near metal severely…
Other Parts Discussed in Thread: MRD2EVM , TRPGR30ATGC , RI-STU-MRD2 , RF-HDT-DVBB Command "start inventory" does not work on my MRD2EVM. Please let me know if I can run the command "start inventory" for the included set of test tags. Otherwise…
Hello Ramon,
We do not have a full turnkey solution for what you've described, but our TI Design for an NFC Reader/Writer system will help get you going in that direction from the NFC side: http://www.ti.com/tool/TIDM-NFC-RW
The TI Design includes…
Athul -
your tags will be too small for an antenna of that size - for your reference some time back i had connected up our reader platform to Feig 300mm x 300mm antenna to check this exact scenario...the problem is basically a tag that small requires…
u-boot-files.tgz.base64.txt
Prashan,
I cant upload file in binary format, so I convert in base64.
Use the following commande to get the archive:
base64 -d u-boot-files.tgz.base64.txt > archive.tgz.
So I include the tisdk u-boot base files, the ethboot…
Hi Mike,
In general, RFID tags that are encapsulated can withstand the higher temperatures required for autoclave. For example, take a look at our high frequency(13.56MHz) overmolded 22mm tags. This can withstand 130C for 50 hours and 220C for 30 seconds…
Until I can get my hands on the code (To source code for the mystery code that works so well) that detects these card I am running more tests here:
Turns out only one model of card works only with the hex code and doesn't work with the SLOC code. …
Other Parts Discussed in Thread: RF-HDT-DVBB This is the first time I have asked a question and am only very new to this community.
I have designed an RFID Tag incorporating the RF-HDT-DVBB 13.56-MHz Encapsulated Plus Transponder. Documentation states…
Daniel -
our RF-HDT-DVBx parts are made to live in such environments such as drycleaning fluid (which is not so different from fuel) but smallest one we manufacture is 22mm in diameter, which is over twice as big as your 13/32" (.406 in or 10.3mm) size…