Part Number: AWRL6432 IWRL6432 AWRL1432 IWRL1432 Other Parts Discussed in Thread: IWRL6432 , IWRL6432BOOST
xWRL6432 and xWRL1432 are ready for evaluation!
Product folder and EVM:
IWRL6432 Product Folder
IWRL6432BOOST EVM
AWRL6432 Product Folder
AWRL6432BOOST…
Hi,
Attached is the RAW image downloaded using DCC with these parameters:
I attached the RAW image and also the VLC image that corresponds to it. The RAW file was renamed to txt since the tool did not allow uploading of a file with extension RAW! AR0331_Date_23…
best.onnx.txt
Hi,
Here is the modeI file. I have tried and found this can only upload txt file. So I modify the suffix. After you download the mode file, you should modify the suffix to onnx. Please help me setting this parameter.
Regards, You
Part Number: CC3200 Tool/software: Code Composer Studio Hi, TI
Now, I use example "mqtt_client_tirtos" from CC3200SDK 1.4
It can't connect with broker follow this configurations.
Please tell me, how to connect broker with this example. …
VGA_out.y.txt customImage640x480.raw.txt VGA.y.txt customImage_output640x480.raw.txt Hi Champs,
I am using CCS 5,4 for EVE simulator. its getting compiled and i tried to run the morphology testcase, it worked fine.
Now i wanted to check with edge detection…
1. The booting of u-boot fails in the SPL before any console output. Is there something else I could provide that would help? 2. The same emif registers values are used for both emif1 and emif2. See attached *.xlsm file for calculation of emif values …
Hi Margaritha,
What could be the reason that mdiscalar and hdiscalar elements behaving differently?
One thing I observed that while using mdiscalar element 2 out of 3 frames capturd are full of grains as shown in the snapshot below
yuv file : (convert…
So i am using the EVM board which has the 16Mhz master clock. I looked at the signals with the oscilloscope and they look good, i also looked at the signals inside the FPGA real-time capture tool and i get the same as the salea... I added NULL commands…
Hi,
I mean I can play it in VLC, but it play not smoothly. when I use the Elecard StreamEye Tools to play it , it is smoothly, i
I have uploaded the video . Because i want to upload the video ,so i have to change the file`s expanded-name to txt, it is not…
Hi Louis,
It looks like one of the redistributables is not installing correctly on your machine. Can you please:
Save the attached file as .exe
Double click on it to run it.
Follow the prompts and report any errors.
If no errors, please delete the contents…