I have followed the steps suggested and i am still facing the same issues with the input , i have added all the plots here for more analysis
comparision_outs.zip.txt
Fullscreen
tidl_importfp32.txt
Download
modelType = 2
numParamBits…
Hi,
We are using the SK-AM62 E3 revision. Can you please confirm which revision are you testing the HDMI audio?
Shorted the j24 pins. Still HDMI audio is not coming.
Attached the boot logs for you.
Fullscreen
5367.Bootlog.txt
Download…
best.onnx.txt
Hi,
Here is the modeI file. I have tried and found this can only upload txt file. So I modify the suffix. After you download the mode file, you should modify the suffix to onnx. Please help me setting this parameter.
Regards, You
Hi Margaritha,
What could be the reason that mdiscalar and hdiscalar elements behaving differently?
One thing I observed that while using mdiscalar element 2 out of 3 frames capturd are full of grains as shown in the snapshot below
yuv file :…
u-boot-files.tgz.base64.txt
Prashan,
I cant upload file in binary format, so I convert in base64.
Use the following commande to get the archive:
base64 -d u-boot-files.tgz.base64.txt > archive.tgz.
So I include the tisdk u-boot base files, the…
Hi,
I mean I can play it in VLC, but it play not smoothly. when I use the Elecard StreamEye Tools to play it , it is smoothly, i
I have uploaded the video . Because i want to upload the video ,so i have to change the file`s expanded-name to txt, it…
Hi Stefan,
I've attached the zImage and the modules for the corresponding image. Please try this out and let us know if it works. Copy the zImage to the boot folder in the rootfs partition and the modules to the lib/modules folder in the rootfs partition…
Could you please try the following:
1. Download the file attached. Change the extension from .txt to .bin
2. Run it from the command line with the following parameters:
"ti_simpack_vayu_ccs_0.6.2.0_setup.bin" --mode silent --prefix "/home/vasanthaangappan…
Hello Hideaki,
I'm not too familiar with these labs, but I do have a couple of BIOS examples for F28377D that use controlSUITE. These examples use IPC to send messages between CPU1 and CPU2, though, which may be more than what you are trying to do.…
Hi Nikshith,
Please use the below attached files - 8865.txt 2364.txt Rename the above RAW video files from .txt to .yuv (e.g 8865.txt to 1.yuv & 2364.txt to 2.yuv) Create the input raw file combination of black and actual raw video -
cat 1.yuv 2.yuv…