Other Parts Discussed in Thread: CC2564MODN , CC2564 5875.Range Estimation for Indoor and Outdoor Rev1_12.xlsx
Hi,
The attached excel sheet helps to estimate a practical range estimation for indoor and outdoor radio links.
The outdoor is based…
Hi,
We have several customers using sub-1 GHz for these type of applications.
1. In order to start the SW evaluation, please refer to the CC110L examples here: https://www.ti.com/tool/download/SWRC219 or the simple CC1101 examples here: https://www…
Other Parts Discussed in Thread: CC430F6137 , CC430F5137 Dear All,
I would like to use RF communication module of TI cc430F6137. How can I do it? Any reference link? what is the diameter range of RF signals for this?
Thanks & Regards
Bhavdips…
Other Parts Discussed in Thread: CC2650 , CC2590 Hi,
I am using CC2650EM with smartRF06 and the new SensorTag, and would like to improve the RF range communication.
My setup is as following:
CC2650EM with smartRF06 - Running SimpleBLECentral.…
Other Parts Discussed in Thread: CC2538 Hi
In my project, we used cc2538DK. Here externally we interfaced fingertip heartbeat sensor on smartRF06 board.
we consider one as end device and other as coordinator.....using RF the sensors data is communicated…
Hi Malcolm,
Thanks for posting on the E2E forum. What is the distance from the house to the garage? I assume you only want to work with two devices, a transmitter and receiver, which communicate over-the-air so that your switch application can respond…
Hi,
A1, A2 and A3 is a pi-network for antenna matching purposes. A1 is not needed for this board so it has been marked as DNM which stands for Do Not Mount.
The antenna on this board has good performance so it is not automatic that using an external…
Francisco,
Francisco Zamudio said: My main concern about the antenna selection is that it won't support the distance that I am looking for (about 100m).
There are many factors that can affect the maximum range of a system, starting with the antenna…
Other Parts Discussed in Thread: LMH2110 My customer is looking for a low power RF detector. I found this device (lmh2110) but seems to fall short on the RF input power range. We do meet the freq range.
Can you tell me if we have anything else that…