As you can see from http://www.ti.com/tool/rf-range-estimator the range will be limited when the noise in the used channel/ center frequency is high. If possible you should select a different channel that Bluetooth/ WiFi operate on. The used channel is…
Please check the IPC chapter in https://www.ti.com/lit/pdf/swra640 on which IPC you can use with which part. I would change the IPC to ensure that you use all ports.
Using an IPC will typically give slightly lower performance than a discrete design…
Have you calculated the estimated range with www.ti.com/.../RF-RANGE-ESTIMATOR ? You can also use www.ti.com/.../swra603 to debug range. You are not saying anything about the hardware you are running on which makes it not possible to say if you get the…
Hi Mike,
Q1) What about choosing the project dmm_154sensor_remote_display_oad_lpstk_app ?
Q2) I let you run a few more tests :) In addition, I am not sure if you are using the right mobile app (on your screenshot I recognize the one dedicated to the…
As you can see from www.ti.com/.../rf-range-estimator , range decreases when the antenna is close to ground which in effect the skin is.
I would check the conducted output spectrum with a spectrum analyzer with and without the decoupling caps and see…
Hi,
AOA relies on a BLE connection. If the BLE connection can occur than AOA will be possible. As a result, 5m is definitely possible. If you want more details on the BLE range, please use RF-RANGE-ESTIMATOR .
When it comes to AOA accuracy, it mainly…
a) I doubt it. Play some with http://www.ti.com/tool/RF-RANGE-ESTIMATOR to see what is required. Note that in the tool it's the dB numbers that are important. Select a chip/ setting that gives close to the datasheet sensitivity of CC2500.
b) Yes and…
You can use www.ti.com/.../RF-RANGE-ESTIMATOR if you want a more accurate estimate if not already done.
A module should be able to be run with any phy if it's not chipped with a stack and hence the phy layer is not possible to change.