Part Number: RF430F5978 I Have a question during the development ID key use RF430F5978.
Current WAKE Pattern detection: work with and develop your will be Behavior 1) WAKE pattern A of detection: WAKEInterrupt pin detection, wake-up, After the interru…
Part Number: RF430F5978 Hi,
I have a question about the switch interface function of RF430F5978.
What kind of situations is this function used in?
What can I do with these eight switches? SW(7:0)
Best regards, Seishin
Part Number: RF430F5978EVM Hello,
I am attempting to pass a long address from the ID Tag from the MRD2 to the RF430F5978 using the Data after Wake feature described on pag. 771-3 in the SLAU378. When I attempt it, I cannot capture more than four additional…
Part Number: RF430F5978
Hello team,
Hope you are well.
Please see below question from the customer:
I have looked at SLAU378 section 24.11.3.4, is there another location where I can find more information on how to select the trimmer capacitors? And…
Other Parts Discussed in Thread: RF430F5978 Hello,I want to know recommended UHF antenna for RF430F5978.
Now I try to design PCB integrated RF430F5978 for evaluation.
There is only circuit information RF430F5978EVM document(slru007.pdf).
I want to know…
Other Parts Discussed in Thread: RF430F5978 , CC1101 , TMS37F128 Good morning,
we are considering a project involving this part with an important modification :)
We would like to know if it would be possible by HW and / or SW changes to shift the operational…
Other Parts Discussed in Thread: RF430F5978 Hi,
I want to know how the LF antenna trimming of RF430F5978 when mass production.
I think there are two ways.
①Wired : By use of RI-ACC-PTB2 via the probe test interface. ②Wireless: By use of "LF ANT Trimming…
Other Parts Discussed in Thread: RF430F5978 Is it possible to use the RF430F5978 in a total batteryless construction? I have to send a short message on the 1 GHz radio about 10 times a second (each time the LF radio is activated on the reader). On the…
Hi,
How long does it takes to wake microcontroller up from 3D LF reader in the worst case?
I mean absolute time (ms) for Wakeburst + SOF + Wake Pattern (24 bit) + EOF
Other Parts Discussed in Thread: TMS37157 Could the microreader2 talk to the LF radio in the RF430? Also the datasheet mentions that the RFID transponder is a TMS37206? I suppose this would have similar functionalities as the TMS37157?
Also on a somewhat…