Part Number: RM46L430 Tool/software: Hi team,
According to the data sheet, the rise/fall time between VIL and VIH is specified as tin_slew=1nsmax.
Q1: Does it mean that the rise/fall time of the input voltage to the MCU has to be less than 1ns?…
Part Number: RM46L430 Hello, We currently using target device RM46L430. SafeTI-HALCoGen-CSP file access for use with RM46x can you help me? TI NDA has already been signed.
Part Number: RM46L430 Hello,
We are preparing for SIL2 certification. I would like to refer to the SafeTI related document SPNU570. Can you help me obtain this document?
Best regards,
keon Young
Part Number: RM46L430 Hello,
We are doing SIL2 certified development using the TI RM46x. Can I compile and use the SafeTI Diagnostic Library in Keil MDK?
Best regards,
Keon Young
Part Number: RM46L430 Other Parts Discussed in Thread: RM46L450 , RM46L830 , RM46L852 , RM46L850 , , RM46L840 , RM46L440 Hello
Could you update the following SIL certificate?
The expiration date has expired.
https://www.ti.com/lit/cr/spnq001c…
Part Number: RM46L430 Other Parts Discussed in Thread: HALCOGEN Hello,
I have difficulties with SPI slave on RM46.
Do you have an example or a tuto for SPI slave on RM46 ?
Thank you on advance.
Regards
Part Number: RM46L430 Hi, we are using the following design to read a 24V digital signal into the RM46L430 on digital input:
Unfortunately the 3,0V-Z-diode is missed on some PCBs. On these PCBs the input of the RM46 is now driven by 4.0V. Tha means…
Part Number: RM46L430 Other Parts Discussed in Thread: HALCOGEN
I'm trying to use GNU tools to compile the HALCoGen code for RM46x micro. I've set the option in HALCoGen and it is correctly outputting asm and c files which I can compile. What am I supposed…
Part Number: RM46L430
Is the concern and need to back up and restore SRAM before SL_SRAM_TEST as described in this post:
https://e2e.ti.com/support/microcontrollers/hercules/f/312/p/601225/2215521
still applicable for STL version 2.40?
Was the…
Part Number: RM46L430 Hi Sunil, Customer is a bit disappointed with the value 1.58 CoreMark/MHz. According to ARM website, Cortex-R4 is 3.47 CoreMark/MHz which is more than double. https://developer.arm.com/ip-products/processors/cortex-r/cortex-r4 As…