Part Number: RM46L850 Other Parts Discussed in Thread: HALCOGEN Tool/software: Code Composer Studio Hi
how can I capture input signal and to measure duty cycle which is coming from external source.
capturing should carried out via HET port pin.
…
Part Number: UNIFLASH Other Parts Discussed in Thread: RM46L850
I want to flash program to TI IC (RM46L850) by NI LabVIEW to control the UNIFLASH programmer for IC's erase,blank check,program,checksum check,verify.
my question:
Can I control the…
Part Number: TMS570LS1224 Other Parts Discussed in Thread: RM46L850 I tried the demo video https://youtu.be/WYjLGBr9n3M to generate PWM on Hercules TMS570LS12x LaunchPad (RM46L850) but it is not generating any PWM signals.
I will never recommend operating a part with less than the recommended requirements as defined in the datasheet. (I am assuming 144 QFP as you did not mention if you are using QFP or BGA). For the RM46L850 starting in section 4.3.1.15 of the datasheet…
Hi,
I'm currently working with the RM46 and TMS570. I'm trying to understand the EMAC module.
In section 31.2.17.1.1 of RM46xx datasheet, it is stated that " the EMAC issues an interrupt to the CPU when it writes the packet’s last buffer descriptor…
Hi Jagadish,
First of all, thanks for the help.
Below is the TUV SUD certificate search data. What we need is a certificate and a test report.
Best Regards,
keon-young lee.
-------------------------------------------------------------
…
Hello,
From what I can see in MCP23S17 datasheet you can use RM46L850 with Polarity 0 Phase 1 (Figure 27-9 from RM46L850 TRM. All modes are described in Table 27-2).
Communication protocols and registers for MCP23S17 are described in MCP23S17 datasheet…
Hi Mathias,
Please refer below thread, here QJ highlighted the pins required for USB connection.
(+) RM46L850: USB example code not working - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
-- Thanks & regards…
Other Parts Discussed in Thread: RM46L830 , RM46L852 , RM46L850 , RM46L430 , RM46L450 , RM46L440 , HALCOGEN Dear Sirs,
We need to design a product for industrial applications with SIL 3 rating according to IEC 61508.
The system must be composed of…