Part Number: RM48L530 Hello Champs,
Customer has already got v1.2 FMEDA document.
Would you please kindly suggest whether the testing datat in it are only applicable to automotive application or also covering other applications? Thanks!
Best Regards…
Part Number: RM48L530 Other Parts Discussed in Thread: TMS570LS20216 Device: RM48L530
IDE: IAR 8.11.3.13984
Compiler: IAR 8.11.3.13950
OS: Sciopta 1.9.15.10
Hi,
I'm trying to implement a fault insertion test for RAM ECC on the RM48 and have modeled my…
Part Number: RM48L530 iHello,
I want to know the pin status while and after reset (nRST was driven low) of the following pins. It is for a SIL-2 circuit.
ECLK (in standard operation we generate 1MHz clock for external cuicuit through this pin). Should…
Hi Bendan,
I was expecting that it was an independent clock generation circuit similar to a frequency generator but not one specifically, The device is fully capable of operating with an external clock source applied to OSCIN as you have indicated so…
Part Number: RM48L530 Dear sir / madam, hopefully a quick question regarding the Hercules range of Safety Micro controllers. We are in the process of designing a Safety Controller for an Elevator System adhering to IEC 61508 standard. As far as we are…
Part Number: RM48L530 Other Parts Discussed in Thread: HALCOGEN Tool/software: Code Composer Studio Does Tivaware or Stellarisware support the RM48L530 MCU
Hello Winfried,
Sorry for missing this post from August. See my comments for your questions:
1.) how does the nERROR pin react while a possible diagnosis. Is there a special diagnosis possibility foreseen in the CPU?
How could that be? Is it possible…
Part Number: RM48L530 Other Parts Discussed in Thread: HALCOGEN Hi
Our application uses the Halcogen generated selftests (run in sys_startup.c). Among these tests are the PBIST test, followed by a memoryInit. Unfortunately we have defined sections in the…
Part Number: RM48L530 Other Parts Discussed in Thread: HALCOGEN Hi,
The TI FEE driver seems to not be able to write to the flash after a software reset.
We are using the TI FEE driver provided with HalcoGen v4.06 and using F021 Flash API v2.01.01. The…
Part Number: RM48L530 Hi TI,
After compiling ARM project,there are .out file,.map file and .hex file.
I want to know what's the relationship between them?
And how to read a .hex file,what's the key factor of .hex file,what informations can we get…