Part Number: RM57L843 Other Parts Discussed in Thread: HALCOGEN Hi team,
I have doubt on EMAC Clock, Which clock domain is used for Ethernet module VCLK3 or VCLKA4_DIVR?
Because In TRM VCLKA4_DIVR is used for EMAC internal logic but In data sheet VCLK3…
Part Number: RM57L843 Other Parts Discussed in Thread: HALCOGEN , DP83640 HI TI Team,
I want to interface between RM57L843 MICROCONTROLLER WITH LAN9354I/ML CHIP .
Please guide me to what are the steps to follow.
Thanks and Regards,
A. Ajith Kumar
Part Number: RM57L843 Hello,
I made absolutely no progress since three months ago when I asked for the confidential RM57L843 Safety Analysis reports and have been redirected from this forum to direct contact with sales team in order to sign the necessary…
Part Number: RM57L843
HI TI-Team,
Kindly Provide me the example code for software reset on RM57L843 controller in register SYSECR and SYSESR.
Thanks in advance,
Regards,
A. Ajith Kumar
Part Number: RM57L843 Hi, TI team.
This is a very basic question, but I haven't found a way to do it. I want to import the SafeTI Diagnostic Library (v2.4.0) in my application and use its functions. I would like to know which is the first thing I need…
Part Number: RM57L843 Other Parts Discussed in Thread: LAUNCHXL2-RM57L , HALCOGEN HI TI Team,
I want to work with an RMII Interface on LAUNCHXL2-RM57L Development board. By Default it was setting as to work with an MII Interface. What are the changes have…
Hi WBLee,
Actually, calling address 0x0000 0000 is not an ideal method to reset the bootloader, because if you did like this then your bootloader initializations will not happen properly because the corresponding RESET flags will not SET.
I mean if you…
Dear WB
Thank you for your great help. I wasn't referring to " run an application after writing it to Flash in the Bootloader, " I know that. My problem is after jumping to the application using g_ulTransferAddress = (uint32_t)APP_START_AD…
QJ Wang said: 1. Please make sure there are good power supplies to MCU (3.3V, and 1.2V).
Yes, There is a good power supplies 3.3V and 1.2V.
QJ Wang said: Are nPORRST and nRST released from reset state?
Yes,nPORRST and nRST was released from reset.
QJ Wang…