Part Number: TPS6594-Q1 Hello,
I was connecting to an external PMIC via the I2C connections on the EVM platform. I was able to sucessfully connect via I2C where I could read and write registers in the Scalable PMIC GUI. I was then able to sucessfully…
Part Number: TPS6593EVM Other Parts Discussed in Thread: SCALABLE-PMIC-GUI , Tool/software: from where we need to download the GUI composer runtime for TPS 6593 part
Hi yang,
Is this a functional safety application? It sounds like you are wanting to do a custom configuration rather than using the catalog PMIC device configuration for the AM62A? If you have the GUI you can use it to reprogram the part for development…
Part Number: TPS65037EVM Error message
Error:Failed to connect: InvalidAgentVersion: Installed version is out of date
I am using ticloudagent_2.
I successfully use theTI Scalable PMIC GUI
Part Number: TPS6594EVM Hi,
I am using TPS65941111EVM, it does not connect to Scalable PMICs GUI,
I use I2C, but it deos not work, I follow the guides to make jumpers correctly I think.
can you tell what may be wrong?
Thanks
Max
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: TPS6594EVM , I'm blocked while trying to program the NVM of a TPS65940 on a custom-designed board using the Scalable PMICs GUI. Looking for guidance on how to proceed.
■ Error message "Device…
Part Number: TPS6593-Q1 Other Parts Discussed in Thread: SCALABLE-PMIC-GUI Tool/software: we are seeing similar issue to this where we are getting 15 pulse during startup but there is no output.
TPS6593-Q1: PMIC Ouput are not coming - Power management…
Hi Max,
1. Various interrupt events are able to keep the system from booting properly. To better help with your issue, can you please provide the following:
Register Dump (main items of interest are INT registers: 0x5A to 0x6C
2. You can jumper…
Part Number: TPS6594-Q1 Hi TI Experts,
Setup
Custom board with a blank TPS65940400RWERQ1
GPIO3/4/10 pulled down on the board (I2C mode, no CRC, address 0x28)
Programmed through the Scalable PMICs GUI v5.0.0 with an AEVM controller
What…
Hi Atsu,
Please read the scalable PMIC GUI user guide for more details on how to configure the NVM.
Scalable GUI user guide : Link
Application note on the NVM update : Link
Also can I ask why are you evaluating this PMIC?
Regards,
Ishtiaq…