Part Number: SCANSTA111 Tool/software: Hello,
I am asking about thermal resistance data for your part SCANSTA111MT.
I see on the datasheet this component has a θ JA of 85 °C/W. Do you have data for the θJ B or θ JC please?
Kind regards
Da…
Part Number: SCANSTA111 Other Parts Discussed in Thread: SCANSTA112
We need to configure the SCANSTA111 in transparent mode (including the 3 chain, not only one). We used to have the SCANSTA112 and we were able to do so using the command TRANSPEN. However…
Part Number: TMS320C6747 Other Parts Discussed in Thread: SCANSTA111 , , SCANSTA101 Dear Team
One of my customer wants to use SCANSTA111 to make JTAG bridge to interface FPGA and C6747 DSP. They are able to load the code to FPGA but not DSP. They can…
Part Number: SCANSTA111 Hi,
I could not find IBIS file for SCANSTA111SM in TI website, please anyone from technical team provide us this file, so
that it would be helpful for us in performing signal integrity analysis in our board.
Thanks & Regards…
Hi Michael,
I searched through our internal archives and am unable to locate a SCANSTA111 IBIS model. The SCANSTA112 is a superset of its predecessors: SCANPSC110F and SCANSTA111. All features and functions that the SCANSTA111 uses can be produced by…
the data sheet states that the default value of the Mode Register0 is 00000001 (LSP0). I have a design that has JTAG resources on LSP2 which requires Mode Register0 set to 00000100. I am looking for a svf example of this programming.
Hi.
Do you have in mind to include 1.8V / 2.5V compatible outputs to existent functionality of these chips? And maybe smaller footprints (e.g. BGA with .5 mm grid)?
Maybe we could buy about 1ku of 111s, and some 112s, but 1.8V compatibility is an…
Part Number: SCANSTA112 Other Parts Discussed in Thread: SCANSTA111 , Hi team,
My customer would like to use this device and they are wondering if there are known erratas for the SCANSTA111 & 112.
Thanks in advance for your feedback,
Regards,
…
Allan
I want to provide a forewarning here that the support for JTAG devices is limited, as the original National Semiconductor group who supported this product no longer exists, thus limiting our in-depth knowledge about this device.
SCANSTA112 would…