Dan
Here is the thermal model info for SCANSTA111MT.
For Analysis Requests, please add further description Result- Theta JA-High K (standard datasheet value) 53.1 Result-Theta JC, top (standard datasheet value) 13.5 Result-Theta JB (standard datasheet value…
Part Number: SCANSTA111 I have a problem this the TRSTB signal.
Whenever I want to pass through this signal to any Port of the SCANSTA (TRST0-2) The SCANSTA loses his configuration and supprotre not this signal.
I need the Reset Signal for the prozessor…
Part Number: TMS320C6747 Other Parts Discussed in Thread: SCANSTA111 , , SCANSTA101 Dear Team
One of my customer wants to use SCANSTA111 to make JTAG bridge to interface FPGA and C6747 DSP. They are able to load the code to FPGA but not DSP. They can connect…
Part Number: SCANSTA111 Other Parts Discussed in Thread: SCANSTA112
We need to configure the SCANSTA111 in transparent mode (including the 3 chain, not only one). We used to have the SCANSTA112 and we were able to do so using the command TRANSPEN. However…
Part Number: SCANSTA111 Hi,
I could not find IBIS file for SCANSTA111SM in TI website, please anyone from technical team provide us this file, so
that it would be helpful for us in performing signal integrity analysis in our board.
Thanks & Regards
…
Other Parts Discussed in Thread: SCANSTA111 , SCANSTA112 Hi team,
the device DS references an IBIS model for this part but there isn't one on the product folder, nor is there one in the large IBIS package. I see 101 and 112, and a note in the 112 that…
Part Number: SCANSTA112 Other Parts Discussed in Thread: SCANSTA111 , Hi team,
My customer would like to use this device and they are wondering if there are known erratas for the SCANSTA111 & 112.
Thanks in advance for your feedback,
Regards,
Pol.
the data sheet states that the default value of the Mode Register0 is 00000001 (LSP0). I have a design that has JTAG resources on LSP2 which requires Mode Register0 set to 00000100. I am looking for a svf example of this programming.
Hi.
Do you have in mind to include 1.8V / 2.5V compatible outputs to existent functionality of these chips? And maybe smaller footprints (e.g. BGA with .5 mm grid)?
Maybe we could buy about 1ku of 111s, and some 112s, but 1.8V compatibility is an issue…
Other Parts Discussed in Thread: SCANSTA112 , SCANSTA101 , SCANSTA111 Hi Team
My customer Zhuzhou would like to use SCANSTA112 for multiple Jtag programming, but both I and customer don't have any ideas for this device, so I'd like to check with you for…