Part Number: SCANSTA112 Other Parts Discussed in Thread: SN74CB3Q3251 Hello Team, We are designing a product that follows backplane architecture. Each daughter PCBs (that are connected to the back plane) will be connected to some DUTs. We need to update…
Part Number: SCANSTA112 Other Parts Discussed in Thread: TMUX1309 , SN74LV4051A , TMUX1308 , TMUX1574 Hello,
We are planning to use SCANSTA112 IC as a switch/multiplexer for parallel programming of multiple boards through any debugger.
Can this IC be used…
Part Number: SCANSTA112 Other Parts Discussed in Thread: SCANSTA111 , Hi team,
My customer would like to use this device and they are wondering if there are known erratas for the SCANSTA111 & 112.
Thanks in advance for your feedback,
Regards,
Pol.
Part Number: SCANSTA112 I have a SCANSTA112 device between a FlashPro Lite programmer and a ProASIC Plus device I am trying to program. My programming plan is to first place the SCANSTA112 into full transparent mode. Then I should be able to connect up…
Part Number: SCANSTA112 I need to configure this TI JTAG Multiplexer (SCANSTA112) in Scan bridge Mode (using the JTAG port). My only JTAG tools are from the Intel Quartus Prime and Micro Semi Flash Pro tools. These tools are FPGA specific and I don't…
Part Number: SCANSTA112
I am trying to implement a configuration like the image below for JTAG. I have a requirement to only connect to 1 FPGA at a time and there is no bus or chain on any of the target devices.
Each would be selected using GPIO lines…
Part Number: SCANSTA112 Other Parts Discussed in Thread: SCANSTA101 , Hi Team,
My customer had a project the HW adopt SCANSTA101 and SCANSTA112 to implement JTAG chain for the CPLD program.
SCANSTA101 will link with main CPU be JTAG source. They have some…
Part Number: SCANSTA112 Tool/software: Code Composer Studio Good day colleagues,
My customer is using the SCANSTA112 but can't use it fully with the XDS200 programmer.
Could you help to understand if it's possible to use CSS or maybe another utility…
Part Number: SCANSTA112 Hi,
we want to use the B0/B1 ports with external connections (i.e. USB JTAG adapter) and are are wondering if additional ESD protection is needed. The datasheet states that there are NO ESD clamp diodes on the corresponding input…