Part Number: TMS320F28P550SJ
Hello!
Thank you for your interest in the E-Metrology Library for F28P55x and F28P65x. If you are interested in knowing more about how the metrology parameters are calculated and the mathematical formulae used to do please…
Thanks for the advice.
Now it works.
I knew about the post_build generator but I think that using it by prompt was very confusing.
Using it inside CCS ( Project properties->CCS Build->Steps->Post-build steps ) it's very easy.
Hope to see this…
Both the x-loader and U-boot included in the SDK do specifically function with the OMAP3530 EVM, it is possible that any necessary updates from the SDP just never had the note updated to say so.
Note that the OMAP34x is very similar to the OMAP35x,…
Hi,
Make sure you are following below steps (if you are missing any)
1. While flashing with UniFlash,
a. SOP2 jumper must be connected
b. Don't remove any other default jumpers
c. when it says --please restart device-- and waits, then press…
Hi Kel
I'm seeing following message where I cannot flash my CC3200LP using Uniflash for Blinkey code (.bin file which I've already parsed using CCSv6)
[13:37:33] Begin Format operation.
[13:37:34] INFO: > Executing Operation: Connect
[13:37…
Hi,
We have following hardware setup am3352B series processor with external PCF8523 rtc chip, kernel version is linux-3.12.10-ti2013.12.01, and TI-SDK v7.
We are setting rtc alarm from an user space application using RTC_SET_ALARM ioctl. We could…
Maynard,
Maynard Cabiente said: Both boards are using U-Boot version based on EZSDK 5.05.02.0.
Note that latest version of EZSDK that is tested on AM387x device is EZSDK 5.04.00.11, so could you check with the u-boot from that EZSDK.
LINUXEZSDK…
Thank you Biser
What about Linux?, does Linux have a driver for this unpopulated driver in the EVM?, is the software driver integrated into the Linux SDK provided by TI?, is there an example or demo with a working capacitive touchscreen using this EVM…
Part Number: AM5728
Tool/software: Linux
Board: AM5728
SDK: 3.1.0
I am trying to use OpenCL for some video processing frames from V4L2 and OpenGL to render processed frames, then again send rendered frames to OpenCL/DSP to process them there.…
Part Number: TDA2 Tool/software: TI-RTOS Hi Sir,
Now we are using TDA2x part number is TDA2SXB T QABCQ1 to implement TIDL OD, LD and TSR, but could we use TDA2SGB R QABCQ1 (only 1xA15, the rest of functions are the same) or lower version (e.g. TDA2HGBRQABCQ1…