Part Number: DRA75
Tool/software: Linux
hardware: VAYU EVM XC5777X REV H
software: ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03
PDK: pdk_dra7xx_1_0_10
I want to share the system timer2 to ipu1 as readonly.
I test like bellow…
Hi,
I use idkam437x with ccs 6.1.2 and sdk 2.1.1.2.
I configured the ADC0 module to be triggered by PRUICSS1 EVTOUT0. Everything worked fine until I set the ADC0 configuration to save ID tags of my measurements with a command:
TSCADCStepIdTagEnable…
Pavel , wanted you to know that:
I am working with ccs5 .
The SDK we are working with is DVRRDK_04.01.00.02 .
In previous projects based on the C5510 we worked our audio with no frameWork just:
- Set ‘MCBSP’ regs ,
- Set ‘DMA’ regs ,
…
Hi,
Recently, I build a CCS project used to process the PUSCH transmitted bit, but the CRC attachment of PUSCH is incorrect.
1. Does BCP support the bit-level processing of PUSCH transmission chain? Since as stated in the BCP UG sprugz1, the BCP is…
Lokesh,
sorry, but I don't understand the question. What are you trying to accomplish?
What protocol do you need and how are your devices connected? You really need to provide a bit more of information if you expect anyone to help you.
Also please…
If you have NOR flash in the design which processor can address and cache in to L2. You can lock the cache except 1-way (32KB) and use it like fast internal memory. SYS/BIOS has APIs to do cache locking and this feature is demonstrated in industrial sdk…
Harshit,
Harshit Jain said:
1) How to make the new project by keeping the original source files of stellaris ware intact. I want the copy of source files to be in my workspace.
Stellarisware example projects have library and include linked…
Hi Francois,
Thanks for your advice and information.I will start from the source code and then
find out how to support cc2560 in the sdk.
Best Regards
Ming
Hi Luigi,
hasn't windows 8 a LARGE, I mean LARGE support for BLE?
Check the links in:
http://stackoverflow.com/questions/16952487/windows-8-bluetooth-low-energy-api-example
You do need a second BLE device, and CC2540 USB dongle is one, but if…
Hi Yihe,
Thanks for the comments.
Is this SDK package contains H264/MJPEG/MPEG4 encoding/decoding functionality in the form of library ?
Are there any API's available for the same?
thanks,
Amol Borawake