Please see here:
http://processors.wiki.ti.com/index.php/Device:AM335x:Device_Evaluation
1. The larger package is required if you need two Ethernet ports from the gigabit switch. And yes, having two ports means the switching capability is also available…
Part Number: AM5728 Other Parts Discussed in Thread: DRA752 Tool/software: Linux Hello,
We are using SDK TI-SDK-4.0.0.4-kernel-4.9.28 and when kernel boots up we see the below crash dump.
Could you please help us understand what might be the problem…
Part Number: CC2540 Hi Team,
I have encounter some errors from the field regard the performance of the device while doing OTA process using TI’s stack.
I will appreciate your help, my FW structure relays on the BIM design as given by TI, on the…
Other Parts Discussed in Thread: CC2540 From the CC2540/41 SDK v1.3.1 release notes:
- The HAL SPI driver that was implemented since the v1.3 release can sometimes hang, particularly in cases in which power management is used and when there is heavy…
Benz,
Yes, may be it is better to make a fresh start.
I am using CCS5.4.0 (Linux version), so CCS5 should not be an issue.
I am using the latest EZSDK 5.05.02.00 on Ubuntu 10.04 LTS PC (I have no Windows OS).
For flashing the NAND from CCS, I…
Hi Stefan,
yes, please see https://github.com/beagleboard/am335x_pru_package. There is no official TI support however.
Further support for industrial real-time Ethernet protocols such as Profinet IRT, Ethernet/IP and such are in development and will…
Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 Hello
I am using arago linux with EVM omapl138 -M1 ZOOM Logic.
I've made simple UBT, u-boot and arago distro loading on SPI flash and it works.
I am trying to develop simple i2c transmission…
Hi,
I'm using CC256x Stellaris Bluetopia SDK v1.0 on EK-LM4F232+PAN1323ETU.
I like to know if the current stack support the following setup: - One BR/EDR SPP Server, so that any remote device can inquire and connect to my SPP server. - And concurrently…
Is there a sample application for the driver available?
I found some example code in the sdk:
component-sources/framework_components_3_21_01_26/examples/ti/sdo/tiler/examples/
But it missing some good docementation.
Other Parts Discussed in Thread: TMS320C6678 Hello, can anyone tell me what software I need to program the TMS320C6678 DSP? Do I need Code Composer? My design will be standalone, no Windows or Linux interfacing. Do I need the TMS320C6678 SYS/BIOS SDK…