1. sdk# make distclean ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi-
CLEAN scripts/basic
2. sdk# make ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- da850_lcdk_defconfig
HOSTCC scripts/basic/fixdep
In file included from /home/ilya/TI/arago-2011…
Other Parts Discussed in Thread: OMAP3530 Hi guys!!
I have configured the environment in order to build the sources DSPLINK for GPP and DSP-side. There are errors when I try to do "make" in a prompt of Linux. I show the answer below:
Building kernel…
Part Number: AM5716 Other Parts Discussed in Thread: AM5728
We are making a custom board using AM5716 processor. The board has QSPI NOR memory we are going to boot from. We build a firmware including U-Boot using Yocto system with the official "meta…
Hi James,
we do have WL1271 Linux driver that supports AP. The driver is based on open source driver and we do have SDK for 3 platforms that are based on AM18x, AM37x and AM335x and WL1271 chipset.
Please see our WiKi in http://processors.wiki.ti…
Other Parts Discussed in Thread: OMAPL138 , AM1808 , OMAP-L138 , DA8XX I have an OMAP L138 based system that uses the Davinci-PSP-SDK-03.22.00.02. The system runs a graphics application. After an indeterminate period of time (order of single digit minutes…
Hi experts,
I'm trying to print debug information in Boot Monitor on K2L but failed, please help to suggest what the root cause might be. Thank you.
1 Code package: ti-processor-sdk-linux-k2l-evm-02.00.02.11-Linux-x86-Install.bin, 2 EVM V1.0.2.1 K2L…
Hi,
Adding ANT to a CC2564/67 (BT + ANT chip) is fairly straightforward, and to my knowledge you will not be required to pay additional royalties for using these parts beyond what you would regularly pay your distributor for them but you should confirm…
Hi Yehuda,
Thanks for your post.
You cannot load the example application of AM1808 EVM into AM1707 or OMAP-L137 EVM, obviously it will crash. It cannot be possible.
TI had provided SDK software for OMAPL137 EVM on Linux environment. To develop new…
Hi, I have two queries regarding hardware cryptographic accelerators in DM8148, which are as follows 1 . Dose the DM814x Crypto API Driver (Linux drivers that provide access to the hardware cryptographic accelerators) supports rijndael (with block size…
Part Number: AM3352
Tool/software: Linux
I am using my customer board based on AM3352, DP83867 and for SDK I am using evm-04.03.00.05 which has u-boot 2017.01
when I start DHCP, uboot is crashing with following error.
cpsw Waiting for PHY auto…