Part Number: SK-AM62-SIP Tool/software: Hi
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1446740/am625sip-sysconfig-ddr-subsystem-ddr-component-js-validation-failed?tisearch=e2e-sitesearch&keymatch=AM625SIP%2520DDR#
For…
Part Number: SK-AM62-SIP Tool/software: Hi,
I'd like to import the eval board pcb design board files in to my CAD (Pulsonix) however it appears that the file in the Altium_ASCII folder is not actually ASCII format. If the design was done in Altium,…
Part Number: SK-AM62-SIP Other Parts Discussed in Thread: AM625 Tool/software: Hello all,
We are evaluating using an im219 sensor with AM62SIP and are trying to get a standard format video stream (standard as in MJPEG, etc).
The issue is, of course…
Part Number: SK-AM62-SIP Tool/software: I'm trying to create an .img file to flash to an SD card, to boot linux on the am62-sip. The goal is to keep the ti bootloader etc. And simply boot my own linux partition. I format the .img into two partitions,…
Part Number: SK-AM62-SIP
Hi TI!!!
I want to do a simpler design than the SK-AM62-SIP and I have the following questions?
I see that VDDSHV_SDIO (MCU side) it is powered through a regulator that is configured for 3.3V or 1.8V. However, the SD is…
Part Number: SK-AM62-SIP Tool/software: Hi All,
I am trying to boot the latest debian image for the AM62SIP board.
I have been advised to use the tisdk-default-image-am62xx-evm-11.00.09.04.rootfs.wic.xz image but it does not boot
The boot error…
Hi Tommy
I checked with MCCI team and following was their response
We have support for the board SK-AM62 , and I checked the schematics of both SK-AM62 ( SPRR448.ZIP ) and SK-AM62-SIP ( SPRR482.ZIP ).
Both seems to be same w.r.t the test automation…
Hello Lawrence Cuthbert
Thank you for the query.
Help me understand if there is a reason to refer to SK-AM62?
Please refer to the PDF that lists the available files and zip files contain the files organized in a folder structure.
Downloadable…
Part Number: SK-AM62-SIP
Hello.
I have a question about the SK-AM62-SIP. Looking at the PCB picture, there is a jump wire connected.
The schematic of "SPRR482 — SK-AM62-SIP Design Files Package" doesn't seem to be modified, is that correct…