Part Number: SK-AM62A-LP Tool/software: Hello Team,
Our current MCU-R5 FreeRTOS FW (which is compiled using mcu_plus_sdk_am62ax_09_02_00_38 ) is working on TI PROCESSOR-SDK-LINUX-RT-AM62A (Version: 09.01.00.02) with our custom board (RT-Linux).
Now we…
Part Number: SK-AM62A-LP Tool/software: Hi Team,
We are trying to measure the mtf50 and sharpness kpis but it seems there is a blur layer in the images. We tried with different optics and varied distance but this remains the same. We have also tried…
Part Number: SK-AM62A-LP Tool/software: Honestly surprised this got through QA, it's a simple problem/fix but dev.ti.com/tirex is completely broken without resolving this.
OS: Linux
Browser: Firefox
Screenshots of the issue. You can see that the…
Part Number: SK-AM62A-LP Tool/software: Hi experts,
Linux SDK: 10.00 MCU+ SDK:10.01
Following the procedure in " Load and run example binaries " in the MCU+ SDK Guide, using " SOC Initialization Using SPL " to display the Linux startup screen…
Hi Karthik We checked the cache alignment for source and destination addresses. We came to know that destination address was not cache aligned so we tried to create one dst buffer which is cache alignment and tried to pass the same to standalone function…
Part Number: SK-AM62A-LP Tool/software: Hi, ti expert,
we use SK-AM62A-LP platform, and sdk 09.02.
we use GPMC interface connect to a oled (i-80 mode) module. and use DMA to copy data from frambuffer to oled's gram.
the DMA can work, and oled can…
Part Number: SK-AM62A-LP Tool/software: Dear Linux Experts,
I've noticed that the date functionality is working differently in SDK version 10.01 than in 9.0 or 9.1. My dev board isn't usually connected to access a NTP server and this is also a use case…
Viral Shah said: We observed that modifying the LSC LUT input table values works up to 1200 entries
For AM62A, LSC shall be able to hold up to 5248 LUT entries -- meaning that "lsc_table_width * lsc_table_height <= 5248". In your case, you…
Part Number: SK-AM62A-LP Tool/software: Hi,
We are looking forward to use AM62A34ASMSIAMBRQ1 for our Automotive application. Having queries on evaluation kit as follow:
Availability of SK-AM62A-LP (seems restricted or obsolete on Mouser and Digikey…