Part Number: SK-AM62A-LP Tool/software: Hello Team, I am using below command to get image data from sensor. gst-launch-1.0 -v v4l2src device=/dev/video-rpi-cam0 io-mode=dmabuf-import ! video/x-bayer, width=1920, height=1200, framerate=60/1, format=rggb10…
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi experts,
Q1:Could you please tell me the build environment for the C7x DSP library? Q2:Also, is there any information that goes into more detail than what is provided…
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: SK-AM62P-LP , AM62P Tool/software: Hello Expert,
Board :SK-AM62P-LP
OS : Processor SDK LINUX RT AM62P Debian Trixie - Version: 10.00.07.04
MCU+SDK : Version: 10.00.07.04
Above are my specifications…
Part Number: SK-AM62A-LP Tool/software: Hi,
We have AM62A custom board, we flash the EMMC in 2 options:
1. Flashing the EMMC when the EMMC on the board'
In this option we get "mmc0: mmc_select_hs200 failed, error -110" error on 1/10 pcs…
Part Number: SK-AM62A-LP Tool/software: We refer to Chapter 1.2.3,
software-dl.ti.com/.../Overview_Building_the_SDK.html
Does Yocto automatically generate a cross compiler for compilation uboot、kernel, What paths are generated separately? If it hasn…
Antonio Cattaneo said: At the moment I'm able to reach the 97% of the work before the error on package install
How does it continue from here (log?)?
Currently 1 running tasks (14209 of 14610) 97% 0: tisdk-edgeai-image-1.0-r0_edgeai_8 do_rootfs - 2s…
Part Number: SK-AM62A-LP Tool/software: Hi
In the question of how to burn AM62x using GPMC NAND, how do I generate tiboot3-gpmc.bin, tiboot3-nand_bch.bin, tiboot3-gpmc_bch.bin?
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: AM62P Tool/software: Hello all,
Currently I am using the following setup: Board: sk-am62a-lp MCU+SDK version: 10.00.00.14 Linux SDK version: 10.00.00.8 Now I have a Linux kernel running A53 cores and…
Part Number: SK-AM62A-LP
Tool/software:
Hi, TI experts,
I created a SD Card using balenaEtcher according to 1.1.2.2. Create SD Card using balenaEtcher , The EVM boot and prints normally.
Then, I built u-boot and install to SDCard using sdk top-level makefile…
Part Number: SK-AM62A-LP Tool/software: Hi, TI Experts:
In AM62A 9.2, the jittering problem is happended like below TDA4EN.
TDA4AEN-Q1: Display Jittering problem on R5F - Processors forum - Processors - TI E2E support forums
Could I get AM62A 9.2 QoS…