Part Number: SK-AM62B-P1 Tool/software: Hi, I want to set up Secure Boot using a Yocto build. Can you guide me on how to generate the images using yocto build system? Also, any general information on the differences between normal boot and secure boot…
Part Number: SK-AM62B-P1 Other Parts Discussed in Thread: CC3301 Tool/software: Which kernel driver is used for the CC3301's PCIe on this board?.
Alternatively, which Kconfig configuration macro is it
Part Number: SK-AM62B-P1 Tool/software: Anyone has experience of cross-compiling flutter apps for arm64 on Linux x64 host? Some sources say it's not yet supported, though I saw some instructions for that elsewhere.
Hi Ritapravo, No, it is not. I understand that sound input/output is only valid if the headset is connected to a 3.5mm jack.
Satoshi Shinohara said: Connect the headset to the 3.5mm jack.
I have followed the steps below and there is still no sound. Is there…
Part Number: SK-AM62B-P1 Other Parts Discussed in Thread: SK-AM62B , SK-AM62-LP Tool/software: Hi,
I'm using SK-AM62B-P1 and it could boot from SD card. However, we want it boot from NAND flash.
I just find a guide about flashing linux to eMMC, I couldn…
Part Number: SK-AM62B-P1 Tool/software: After running the below commands in order to build Linux SD card image (see software-dl.ti.com/.../Overview_Building_the_SDK.html)
git clone git.ti.com/.../oe-layersetup.git tisdk cd tisdk $ ./oe-layertool-setup…
Hi Meet,
Thank you for the quick response. Please let me know how it goes on your EVM.
Suraj Singh said: Boot from boot0 HW partition of eMMC:
=> mmc partconf 0 1 1 1
=> mmc bootbus 0 2 0 0
And I want to know one more thing, if I have a completely…
Part Number: SK-AM62B-P1 Tool/software: I'm on a windows machine and I've plugged in the SK-AM62B-P1 via micro usb(via j15) and LD13 flashes briefly then turns off. Then when I plug it in via usb-c (via j13) to power it, it still does not appear in my…
Part Number: SK-AM62B-P1 Tool/software: Champs:.
What is the 16666666 Hz max meaning in the below log?
BR Rio
18.687705] omap2_mcspi 20100000.spi: registered master spi1
[ 18.692298] spi spi1.0: setup: speed 24000000, sample leading edge, clk norm…