Part Number: SK-AM62B-P1 Other Parts Discussed in Thread: SK-LCD1 Hello,
I have a SK-AM62B-P1 with SK-LCD1. I'm trying to receive touch screen events, but nothing I've tried works. The touch screen appears to be connected, but it looks like the device…
Hi Yong,
yong jin gueon said: 5) Rename tiboot3-am62x-gp-evm.bin to tiboot3.bin.
SK-AM62B-P1 is an HS-FS board.
Can you use the tiboot3-am62x-hs-fs-evm.bin instead?
Regards, Vinu
Part Number: SK-AM62B-P1 Other Parts Discussed in Thread: SK-AM62-LP Hello Team,
We have an request from customer to do our testing on new EVB board SK-AM62B-P1 Board for AM62
Can you please confirm us what are the major differences between SK…
Hello,
nitheesh-raptee said: AM62x Keywriter 09 00 00
This keywriter version needs to be used with MCU+ SDK v09.00 only as the keywriter packages are tied to specific SDK versions. If the issue persists even after this, please share the logs from…
Part Number: SK-AM62B-P1 I was inspecting the SK-AM62B-P1 reference board stackup and have a clarification regarding copper thickness.
I have attached two images below:
1.The PCB Editor stackup view of SK-AM62B-P1
2. The official SK-AM62B-P1 stackup…
Hi Mallika,
Which kernel version do you use?
The follow info doesn't seem to match:
Mallika Vignesh said: serial5 = "/bus@f0000/serial@2850000"; serial6 = "/bus@f0000/serial@2860000";
here uart5 is aliased to ttyS5, and uart6 is aliased to ttyS6…
Part Number: SK-AM62B-P1 Tool/software: Hi Expert,
The customer tested the DFU function on sk-am62b-p1, but sk-am62b-p1 did not respond.
Customers have referenced the following link
3.1.2.1. USB Device Firmware Upgrade (DFU) — Processor SDK…
Part Number: SK-AM62B-P1 Other Parts Discussed in Thread: SK-AM62 Hi Expert,
Please help to provide the .syscfg file for the SK-AM62B-P1
I need to change the pins from RGMII to RMII , keeping all other pins unchanged, so the .syscfg file is needed…
Part Number: SK-AM62B-P1
Tool/software:
Dear TI Experts,
I am designing a custom SBC using the AM6254 Sitara SoC , following the SK-AM62B-P1 reference design. To ensure proper signal integrity, I need clarity on the impedance design targets used…
Part Number: SK-AM62B-P1 I am having trouble booting the SK-AM62B-P1 from TI default images, please see my setup below.
Following is the message on debug UART for boot failure
The SD card was created using this image:
The contents of…