Part Number: SM28VLT32-HT Tool/software: Hello,
I'm looking for a replacement device for PN SM28VLT32SHKN. The replacement that is suggested is die where SM28VLT32SHKN is a CFP packaged device.
Thank you!
Part Number: SM28VLT32-HT Hi, please can you advise if you have any of the part above in stock? If not has there been a update in part number as this looks like it's going obsolete.
Part Number: SM28VLT32-HT Dear Sir
I modified the registers values followed the table 6, when I read the values back, the value I read from the address F004 is not 2BC0 or 03C0,
others values are the same talbe 6. why the value I read from address F004…
Part Number: SM28VLT32-HT Dear Sir
1) it works very well when I wrote any data into BANK0 and then erase it. but it was failed to do same thing for BANK1 to BANK7, after I wrote some data into BANK1 to BANK7, I read memory cells, they are still 0xFF, …
Part Number: SM28VLT32-HT
Hi Team,
Customer want to confirm some item regarding core power usage.
1. Reason the core power usage is so high?
2. Is there a way to reduce the core power usage?
According to them, SM28VLT32-HT power usage rating for core seems…
Part Number: SM28VLT32-HT Hello,
Searching for data storage options at high temperatures. Do you offer any other high temp flash devices besides SM28VLT32-HT?
Max ambient temperature: 150°C
Min ambient temperature: -40°C
Regards,
Brett
Part Number: SM28VLT32-HT I see the SM28VLT32-HT cannot be erased above 125C but can new data be stored at an address location that already contains data?
Part Number: SM28VLT32-HT Hello,
I would need some help to understand the meaning of the endurance value of the SM28VLT32. The datasheet reports 1000 cycles.
Is one single cycle considered completed when the memory gets full and then ready to be "overwritten…