Part Number: SN54AC00-SP Hi,
Two years ago I contacted TI for the issues with the SN54AC00-SP IBIS model at 2.5V. It has not been resolved and our customer now needs the model for simulation. Have you got a fix or any updated version for the model?…
Part Number: SN54AC00-SP Tool/software: I found this IBIS sn54ac00w_sp on the TI website, but this one is characterized for 3V to 5.5V. Do you have one at 2.5V?
Thanks,
Lang
Part Number: SN54AC00-DIE Other Parts Discussed in Thread: SN54AC00 Hello,
I would like to request an unencrypted spice model for SN54AC00 and I have tried to use IBIS2spice but get errors (*DEFINE {RTF}=??bad rtr/rtf value??) when attempting.
Could…
Part Number: SN54AC00-SP Hi expert,
For 5962R87549:
Could you please provide the TID(Up to 100krad) and SEL test report to me?
I can't find it form TI official website.
For 5962-87549:
Why does this SP-grade device not need to do SEL test…
Part Number: SN54AC00-DIE Other Parts Discussed in Thread: TINA-TI , SN54AC00 Hello,
I had spice file for SN54AC00 which is converted from the IBIS model, this file is not working if try in the TINA-TI software.
Could you please help me to resolve…
Part Number: SN54AC00-DIE Other Parts Discussed in Thread: SN54AC00 , SN74AC00 , TINA-TI Could you please provide spice ADS simulation model for the SN54AC00 NAND gate and if the model not available then suggest close alternate model which has spice model…
Part Number: SN54AC00-SP Hi expert,
For SN54AC00-SP, TI has SEE "Estimations and Calculations", but has no SEE/SEL test report.
Could you tell me why Estimations and Calculations are used instead of test report to prove that SEL immune to 86 MeV×cm2…
Part Number: SN54AC00-SP Team,
Section 6.2 Recommended Operating Conditions shows input voltage (VI) at a maximum value of VCC. However, under section 1 Features, it says, “Input Accepts Voltage to 6 V.” Which of these is correct? Can the part handle…
Part Number: SN54AC00-SP Other Parts Discussed in Thread: SN54AC14-SP , Hello, I'm currently procuring these part numbers (SN54AC00-SP and SN54AC14-SP), and very soon our company will have to present an Engineering Model for our system.
Can someone…