Hi Francesco,
Unfortunately, we do not have radiation reports for most of our logic space parts.
Here is a list of devices which do have TID ratings:
SN54AC14-SP (TID 50 krad)
SN54AC00-SP (TID 100 krad, SEL 86 MeV-cm^2/mg)
SN54AC00-DIE (TID…
Todd,
In general across all High Reliability product types, our -SP devices are rad hard, or rad tolerant by design or process. This will make them different from their commercial/automotive or mil-ceramic equivalent.
However, the logic -SP families…
Part Number: SN54AC74-SP Other Parts Discussed in Thread: SN54AC14-SP , SN54AC00-SP , SN54AC02-SP , SN54LVC646A-SP Hello,
I’m looking at your space grade logic line for AND gates and D-flip-flops but I don’t see radiation TID numbers for them. Do you…
KPK,
I am not certain the requirements that ebeam sterilization imposes. Likely is its an ionizing dose that will accumulate with each sterilization.
Most of our standard logic devices have fairly low TID performance. I have heard estimates of 8-10Krad…
Hi Rafael,
It looks like that part number on Digi-Key leads to the SN54AC00-SP, which is a radiation hardened quad 2 input NAND gate.
The SN74AC00 will have very similar electrical characteristics to the SN54AC00-SP, obviously without any of the radiation…
Hey Itai,
I see that the TPS7A4501-SP has a shutdown current of 20 uA max. With this in mind I have found the following space devices.
SN54AC00-SP (RHA 100kRad NAND Gate)
SN54AC02-SP (RAD-TOL 50kRad NOR Gate)
SN54AC14-SP (RAD-TOL 50kRad Schmitt…
Other Parts Discussed in Thread: SN54AC00-SP For one of the experiments at Cern in Geneva we need radiation hard electronics. According to AN-926 from Texas Instruments the National's FACT logic family (54ACXX and 54ACTXX) is a CMOS-EPI process and provides…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…