Part Number: SN54AC00-SP Tool/software: I found this IBIS sn54ac00w_sp on the TI website, but this one is characterized for 3V to 5.5V. Do you have one at 2.5V?
Thanks,
Lang
Part Number: SN54AC00-SP Hi expert,
For 5962R87549:
Could you please provide the TID(Up to 100krad) and SEL test report to me?
I can't find it form TI official website.
For 5962-87549:
Why does this SP-grade device not need to do SEL test?
Thanks…
Part Number: SN54AC00-SP Hi expert,
For SN54AC00-SP, TI has SEE "Estimations and Calculations", but has no SEE/SEL test report.
Could you tell me why Estimations and Calculations are used instead of test report to prove that SEL immune to 86 MeV…
Hi Jung,
I have dug around a bit and cannot find any radiation data for this device.
Unfortunately for older parts such as these, there is no documentation available.
Closest thing I can find is the radiation test for the SN54AC00- SP device. These are…
Part Number: SN54AC00-SP Team,
Section 6.2 Recommended Operating Conditions shows input voltage (VI) at a maximum value of VCC. However, under section 1 Features, it says, “Input Accepts Voltage to 6 V.” Which of these is correct? Can the part handle…
Part Number: SN54LVC646A-SP Other Parts Discussed in Thread: SN54AC00-SP Is there any SEE test data for the SN54LVC646A-SP ? It is TID assured but no links to any SEE test data. I would like to know the SET and SEL performance.
Best regards,
Tom
Part Number: SN54AC00-SP Other Parts Discussed in Thread: SN54AC14-SP , Hello, I'm currently procuring these part numbers (SN54AC00-SP and SN54AC14-SP), and very soon our company will have to present an Engineering Model for our system.
Can someone…
Part Number: SN74LVC1G32-EP Other Parts Discussed in Thread: SN54AC14-SP , SN54AC00-DIE , SN54AC00-SP , SN54AC02-SP , SN54AC02-DIE , SN54LVC646A-SP Dear TI Team,
Is there any report/document that contains single event effects information for SN74LVC1G32-EP…