Part Number: SN54LVTH162245-SP Other Parts Discussed in Thread: SN54LVTH162245 Tool/software: What are the orderable part numbers of SN54LVTH162245-SP for
1. Flight Model?
2. Engineering Model ?
Part Number: SN54LVTH162245 With 1OE/n pulled high via a resistor, what is the default logic output of the buffer if the input (say 1A1) is unconnected?
Part Number: SN54LVTH162245 I have a query conerning the 54LVTH162244 & 54LVTH162245 parts from TI on two points that are not explicitly mentioned in datasheets:
1) Do the data (A, B bus) and control (enn, dir) lines of these parts have cold-sparing…
Part Number: SN54LVTH162245-SP
Hi Support,
Please advise the radiation report for SN54LVTH162245-SP.
Else what radiation tolerant level is it qualified to?
Thanks.
Subramaniam,
First I must point out that we do not have a SN54LVT162245A released. We have the following mil temp (54 series) 162245 variants:
SN54LVTH162245, SN54ABT162245, SN54LVTH162245-SP
Here is our official policy on obsolescence.
Below…
Ankita, We do not have IBIS models for these two devices. However, we do have IBIS models for both in the A versions with WD parasitics. For SN54LVTH16244A : www.ti.com/.../slym084 For the SN54LVTH16245A : www.ti.com/.../slym083 Note, both of these are…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…